STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Catching an incomplete transmission

I use the UART on a STM32F7 with DMA. Is there any way to detect a stop of an incoming transmission with an interrupt e.g. with HAL_UART_ErrorCallback? If I expect too many characters or not all characters are transmitted?

DMeix.1 by Associate II
  • 1483 Views
  • 2 replies
  • 0 kudos

Resolved! Temperature errors on STM32F303RC ADC

We have implemented a single ended ADC input to measure a voltage on our board. At low temperatures there is a significant error in the measurement.Going from +20C to -20C, the value we get from the ADC is ~92mV (114 counts) lower than it should be. ...

DBank.2 by Associate II
  • 2060 Views
  • 5 replies
  • 0 kudos

Timer PWM Dithering for each CCRx register?

The STM32G4 series offers dithering to enhance the PWM ratio. My question is, if dithering can be used on ALL the compare channels of the same timer?Specifically, we generate a center-aligned PWM with two output compare channels 180° shifted. CCR1 an...

GAnde.1 by Associate II
  • 994 Views
  • 1 replies
  • 0 kudos

STM32 RS485 Communication does not work as expected

I have a weight cell which replies to specific frames over RS485 (cell contains its own communication protocol). Manufacturer has a software to test the cell so I connect it to my pc using a RS485 to USB converter and I am able to connect to the cell...

0693W000003Pk6SQAS.jpg 0693W000003Pk7KQAS.jpg 0693W000003Q5CqQAK.png
pbdiazam by Associate II
  • 3531 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.