STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32G030F6 I2C2 set to slave mode, it can not work fine.

I am newer in STM32G030 develop.I tried to set STM32G030F6 I2C2 slave mode with PC.Q1.Using "HAL_I2C_Slave_Transmit(); it seems Master (PC) read 8 bytes later and stop. The other data will not read.Q2. If used HAL_I2C_Slave_Transmit_IT(), It only wr...

RSun.1 by Associate
  • 776 Views
  • 0 replies
  • 0 kudos

Can't figure out why RTC wakeup event doesn't work

Hello,I've followed all the steps required to generate and handle a RTC wakeup in the manual, but it still doesn't work. I can't figure out why that doesn't work.The goal of the following code is that, when I click the reset button of my nucleo L152-...

BCora.1 by Associate III
  • 2256 Views
  • 5 replies
  • 0 kudos

Resolved! STM32L412KB clock options

Im using a STM32L412KB for the first time and Im a little confused about the clock options. I can't seem to change the clock speed (input frequency) in cubeIDE, it's always stuck on 8MHz. However I notice there is an internal oscillator - does this m...

deep_rune by Associate III
  • 1103 Views
  • 3 replies
  • 0 kudos

32F051K86 GPIO initialization problem LL_ libraries

I have a bootloader + 1 wire serial uploader codebecause of space restrictions it uses LL_ libraries for initialization.We have different hardware designs, when using PA2 as IO pin it works !when using PB4 as IO it does not !The main program uses HAL...

Adrian.M by Associate II
  • 2105 Views
  • 5 replies
  • 0 kudos

Setting up DMA for UART on the H745 M4 Chip

I'm trying to setup a GPS sensor (UBlox Max8Q) with a H745 Nucleo board using UART DMA using STM32CubeIDE. However, I’m having problems with setting up my board properly. My plan is to eventually do all my data acquisition on the M4 chip and do compu...

How can I search for MCUs that support ETM or ETB?

We are evaluating the use of ETM or ETB but have problems finding MCUs that support those features (or one of them). Sure we can dig into the data sheet of an MCU family but isn't there a possibility to filter for these features in some MCU finder?

FS.1 by Associate III
  • 1024 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.