STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! adc fails to initialize

Board: stm32h753zi nucleoFirmware & CubeMX: latest versionI have configured the adc to continous conversion and DMA output. The initialization fails in main.c in HAL_ADC_INIT. I stepped through the HAL lib and saw that LL_ADC_IsInternalRegulatorEnabl...

mo_krauti by Associate III
  • 5042 Views
  • 18 replies
  • 1 kudos

Error: Unable to get core ID

im using STM32H753VIT6 MCU.I'm try to connect device using SWD in STLINK debugger but it will show "Error: Unable to get core ID" this Msgim checked MCU input voltage,im getting 3.3v .input power is oknow how can i debug this issue.SWD pins properly ...

kesavans by Associate
  • 1556 Views
  • 2 replies
  • 0 kudos

STM32L071CBT6 issue While recieving Input for GPIO pin

 STM32L071CBT6 GPIO PB15 Input Not Responding to 5V Signal from Buck ConverterHello everyone,I'm using the STM32L071CBT6 microcontroller and facing an issue with reading a digital input on GPIO pin PB15.What I'm Trying to Do:I’m using a buck converte...

Hema_56 by Associate
  • 595 Views
  • 1 replies
  • 1 kudos

Resolved! [STM32F405] flash level 2 protection

Hi, I was trying to test the feature of "Level 2 flash lock" on my custom board. I'm having an unexpected behaviour.My total application consists of a bootloader responsable to load an application via CAN BUS through a custom communication protocol.N...

_marco95_ by Associate II
  • 3106 Views
  • 9 replies
  • 5 kudos

Resolved! STM32L031 UID

Hello,I read the UID from STM32L031K6P6 and each device returns the same result: 0x14473332, 0x38363437, 0x0.I read the value from the address given in RM0377 (0x1FF8 0050).Is the address given in RM0377 correct?I am attaching screen shots from CubeP...

NextUser by Associate
  • 1381 Views
  • 2 replies
  • 3 kudos

Resolved! STM32H7 firmware updater

I use the STM32CubeIDE platform and I need to insert into my project a routine that was able to update my firmware.What I need to understand is:I write the routine then I place it into the ITCMRAM and I run it; does it work ?Have I only to load into ...

carloV by Associate III
  • 2390 Views
  • 8 replies
  • 1 kudos

ADC with timers issue on STM32G474

Hi, I have set two ADCs on CubeIDE, for STM32G474CEU6 microcontroller, with DMA transfer. I am using ADC1 with timer 6 trigger out event and ADC3 with timer 7 trigger out event. The thing is, when I use timer 6 for both ADCs,  just for ADC1 or just f...

Roquebg9 by Associate
  • 700 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.