2025-06-05 5:41 AM
Hi,
I was trying to test the feature of "Level 2 flash lock" on my custom board. I'm having an unexpected behaviour.
My total application consists of a bootloader responsable to load an application via CAN BUS through a custom communication protocol.
Now, If I load my application program via CAN (via bootloader), the MCU can not set itself to level2 but remains set to level 1. If I transfer the same application with JTAG, the MCU can set itself to level 2 protection and any attempt to connect to it is correctly disabled. (in level 1 I can still connect by erasing the whole chip content).
To give further informations, here is the code responsable to set level 2 protection implemented:
FM_ClearFlags();
FM_Unlock();
flashSts = FM_CheckProtectionStatus();
if(flashSts == FM_FLASH_NOT_PROTECTED) // check current protection status
{
FM_SetOBConfig();
flashSts = FM_CheckProtectionStatus();
}
FM_Lock();
void FM_ClearFlags(void)
{
FLASH->SR |= 0xE0; // clear the errors RDERR PGSERR PGPERR
}
void FM_Unlock(void)
{
FLASH_Unlock(); // unlock flash to deal with it
FLASH_OB_Unlock(); // unlock option byte to deal with it
}
void FLASH_Unlock(void)
{
if((FLASH->CR & FLASH_CR_LOCK) != RESET)
{
/* Authorize the FLASH Registers access */
FLASH->KEYR = FLASH_KEY1;
FLASH->KEYR = FLASH_KEY2;
}
}
void FLASH_Lock(void)
{
/* Set the LOCK Bit to lock the FLASH Registers access */
FLASH->CR |= FLASH_CR_LOCK;
}
void FM_SetOBConfig(void)
{
FLASH_OB_RDPConfig(OB_RDP_Level_2); // set to 0xCC to enable the level2 protection --> full chip protection. You cant go back to level 1 or 0. Set a number different (like 0x55) means protection of level 1
FLASH_OB_Launch(); // launch the option byte writing procedure
}
I think the code itself works, because it's working flashing via JTAG. So, why flashing through a custom bootloader does not work?
Thanks,
Marco.
Solved! Go to Solution.
2025-06-12 6:01 AM
I think I found out the root cause.
After my bootloader flashes the MCU, the RDP register is set to FF. The library I'm using was using 3 defines for the levels:
level 0 = 0xAA
level 1 = 0x55
level 2 = 0xCC
The library was checking against the level0, but FF was somehow an unespected value.
I changed a bit logic and now seems to work.
Thanks,
Marco.
2025-06-05 8:08 AM
Did you power cycle the chip? I recall there being some checks for the debugger that only get reset after a power-cycle, or something similar like that.
Removing the code that sets RDP2 and then comparing the content of the flash after flashing with each method would let you know if there is an issue flashing.
2025-06-06 12:14 AM
Hello,
yes I power cycled the chip but still the level 1 protection is enabled. I will try to insert a sw reset immediatly after the flash lock procedure. Maybe it helps.
I will also try to compare the flash content but I don't think we have issue with the flashing procedure since the application is up and running.
Marco.
2025-06-06 5:39 AM
If the flash is the same, the behavior after powerup will be the same. The chip doesn't know or care how the flash got loaded.
2025-06-07 12:52 AM
I Also thought that way but wanted to be sure that no erratas talking about this issue are existing. Let me do other couple of tests on Monday.
Other difference Is that the hex flashed with jtag Is produced by a locale build. Instead, the binari flashed through bootloader Is built by and automation server. (Starting from the same commit, thus the same code)
In your opinion, if I convert hex in binary and compare with the other binary (built from server), should I Expect that binary match completly? This Is an other test I can do.
Please let me know if it make sense and thanks.
Sincerly,
Marco.
2025-06-07 6:25 AM - edited 2025-06-07 6:34 AM
> In your opinion, if I convert hex in binary and compare with the other binary (built from server), should I Expect that binary match completly?
If they're built in the exact same way, yes. Sounds like there may be some differences.
Comparing flash content would be the better check IMO.
2025-06-08 3:23 PM - edited 2025-06-08 3:25 PM
Just mind the filler value in the holes (0 or FF) and any padding at the end.
2025-06-10 7:28 AM
Hi,
i removed the server from the possibilities.
I used local build only. I removed the piece of code to enable the level 2 protection.
I flashed the same binary first with Stm32cube programmer (and read back the flash content after flashing).
Second I flashed via CAN Bootloader. After that I read back with STM32 Cube Programmer.
I compared the two flashes read and are the same. Menaning that the process of writing into flash generates the same flash contents.
I have no other ideas.
Could it be an odd behaviour of the chip?
Thanks,
Marco.
2025-06-11 7:03 PM
> Could it be an odd behaviour of the chip?
Yes - in some sense of odd. Try to reset (NVIC_SystemReset) before setting level 2.
2025-06-12 6:01 AM
I think I found out the root cause.
After my bootloader flashes the MCU, the RDP register is set to FF. The library I'm using was using 3 defines for the levels:
level 0 = 0xAA
level 1 = 0x55
level 2 = 0xCC
The library was checking against the level0, but FF was somehow an unespected value.
I changed a bit logic and now seems to work.
Thanks,
Marco.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.