STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Writing and reading QSPI Flash on STM32F746G DISCO

I created my application using the CubeMX. Here are my read and write routines, my QSPI initialization routine, and while loop. I am using the USB to display what is read from the QSPI flash memory. I am writing a string to the memory, but when I rea...

STM32 ADC sample rate

Hi, I'm using adc single channel with interrupt. the sample time is set as 56 cycles, and the adc clock is (108MHz/4=27MHz). So the sample rate is 27MHz/(56+12)=397KHz. I also using DAC to generate a sinewave with the frequency of 1KHz. If what I cal...

0693W000003RduYQAS.png 0693W000003RduTQAS.png
Jshan.1 by Associate
  • 7359 Views
  • 3 replies
  • 0 kudos

STM32F4 Center aligned pwm timer

I configured timer1 for pwm generation center aligned like below in cube ide.I update duty cycle writing directly CCRx register asyncronously in the code.Most of the time pulses are effectively center aligned but sometimes not (nor left or right ali...

0693W000003RkwqQAC.jpg 0693W000003Rkv9QAC.jpg
BRaff by Associate
  • 3539 Views
  • 2 replies
  • 0 kudos

Unable to read correct pulse width using busy loop and timer.

Dear All,Board: Nucleo - H745ZI-QWhat am I trying to do ?I want to measure pulse width of an input signal using a busy loop and a timer. I keep monitoring a pin configured as input , when a zero is detected (by default input is around 3 volts), a fun...

sarojj7 by Associate III
  • 1524 Views
  • 2 replies
  • 0 kudos

ADC only 4Msps?

Documentation say ADC have max 4Msps, but it refer olways to 60MHz to adc (60MHz * 15 cycle = 4Msps) but manual say ADC max frequency is 170MHz, then 170MHz * 15cycle = 11Msps.This clock is different from Fadc (aka adc kernel clock)?https://www.st.co...

MSzaj.1 by Associate II
  • 3602 Views
  • 8 replies
  • 0 kudos

Print SWOTrace in the IDE debugger console from both cores.

Hi,i'm working on a STM32H755II MCU, I followed this guide and setup two debug configurations one for CM7 (that downloads both codes) and one for CM4. I added on the CM7 project the common implementation for printf:int printf_swo(char *ptr) { uint32...

LMoio by Associate II
  • 966 Views
  • 0 replies
  • 2 kudos

Resolved! TIMER OC output using LL

I ran timer OC mode on PA8 (TIM1_CH1) on STM32f407VGT6 using HAL and it works fine. Then I decided to set up it by means of LL and there is not any output on PA8. I checked my code with Example_LL projects of STM32F411RE-Nucleo in ST F4 repository. I...

MTros.1 by Associate II
  • 4811 Views
  • 6 replies
  • 0 kudos

STM32H743 FDCAN Message RAM Configuration

There are several FDCAN peripheral registers on the STM32H743 that hold the starting address of various elements used for FIFOs and filters. Are these addresses relative to 0 or to the physical address of the FDCAN message RAM (0x4000AC00)? The Refer...

jerry2 by Senior
  • 2002 Views
  • 1 replies
  • 1 kudos

STM32F469 wakeup from Standby with RTC

I tried to set a STM32F469 controller into standby mode and wake it up periodically via the RTC on a custom board and on a STM32F469I-Discovery board. I had the problem that the controller only went into standby once, on the following runs it woke up...

Dubit by Associate
  • 942 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.