Any DLMS/COSEM library available for STM32 tagets?
I've seen an old application note on ST website about a DLMS/COSEM library.Is this code still downloadeable?
Ask questions, find answers, and share insights on STM32 products and their technical features.
I've seen an old application note on ST website about a DLMS/COSEM library.Is this code still downloadeable?
Dear community,I plan to use the USART2 of my STM32F407VE board for an IrDA communication (8N1, 115200 Baud @ 8 MHz fPCLK). I started with initializing my USART2 periphery on the register level (I don't use STM32CubeIDE). This seems to work fine. How...
Hi!I would like to make a wav. player using STM32 microcontroller. My first step was to generate a sine wave using STM32F103C8T6, SPI interface and external DAC MCP4921. However, it's not working.I attach the schematic of my device.I wrote 2 versions...
This should be straightforward but I cant get it to work. I simply want to control the GPIO output of pin PG10 on the STM32F769I-EVAL board. I have removed all daughter cards, LCD and the Micro SD card. According to the datasheet, PG10 is connected t...
Hello, I am trying to use DMA with USART to transmit and receive data to buffers in internal RAM.I setup my DMA1_Stream4 as USART3_TX. However, after setting DMA control register, Peripheral address, memory address, number of data to transfer, Enabli...
We welcome everyoneIs there a way to protect uart from being hacked!?For example:I have a device that uses gsm to send sensitive data.Anyone with a simple background can learn the uart pins and then put a logic analyzer or rx probe and then know ip a...
We encountered a big issue with the ADC's in a project.The G4 device has 4 ADC's configured (ADC1, ADC2. ADC3, ADC5).ADC1 and ADC2 are sampled simultanious and triggered by HRTIMER1A interrupt with 4 channels each.ADC3 and ADC5 are in independent mod...
1. can I use FMC to interface with any kind data address oe cs device? 2. The device is not SDRAM or flash or any kind of memory, Does anybody have an experience with that? 3.The device is from the early 90's and works with 5V logic level, Can I use ...
I'm trying to transmit a newer data while the previous transmit interrupt hasn't finished, I simply just call HAL_UART_Transmit_IT again and the result is the first called interrupt will finish its whole job and the second call do nothing, I know the...
I have this scenario:My stm32f0 implements a I2C slave, and I have a raspberrypi with i2ctools as a master.I define a bunch of 16bit wide registers to access in the stm32.Now I wanted to test what happens if the master only reads 1 byte instead of 2 ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.