STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Unable to assign an address to a pointer!

Hi,I am trying to assign an address to a pointer the following way:#define FM_P_ADDR 0x0807F800uint64_t * addr = ((uint64_t *)FM_P_ADDR);However, running the line will direct the execution to the Hard Fault Handler routine.What is happening? What ...

PMach.1 by Senior
  • 1576 Views
  • 4 replies
  • 0 kudos

TSC Group1 unexpected behavior STM32L552ZE

Hi,I have designed a keypad with 11 touchkey's. For this I have used TSC group 1,3,4 and 6. As FW i have used the STM32_TouchSensing_Library and I have a problem. All groups are working ok, sensing touch corectlyexcept group 1. This group has the sam...

CDan.1 by Associate II
  • 656 Views
  • 0 replies
  • 0 kudos

Resolved! Using an oscillator for LSE in battery mode?

Suppose I use an oscillator instead of the suggested resonator for LSE. Will that even work, i.e., will the internal RTC continue to function when in battery mode? I assume that I'd have to power both oszillator and STM32 (using Vbat)?

STM32F7 I2C timing not respected

Hi,It seems that in some events the I2C data setup time (Tsu;dat) is not respected by the MCU.Please let me know if I am wrong.I am using the I2C1 of an STM32F745 at 100kHz with the HAL library.The I2C setup was done using the CubeIDE.When using HAL_...

0693W000004GvbvQAC.png 0693W000004Gvc0QAC.png

STM32 receive ONLY on SPI peripheral

Hi, I've worked a bit on STM32 before (STM32F7 to be more precise), so I have little knowledge about the STM platform. I normally don't need to ask question on forum because Google is a very good professor, but this time I'm not sure to have found en...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.