STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

understanding the I2C peripheral on STM32L412

I want to use the I2C peripheral on my STM32L412C8T6, although I read the reference manual I'm still finding the operation of this peripheral a little confusing. I have a 4 channel I2C 12bit DAC to operate, so I want the I2C to act as a master transm...

deep_rune by Associate III
  • 2584 Views
  • 6 replies
  • 0 kudos

STMh734 GPIO as parallel bits interface

HiI would like to use the GPIOs on the STMh743 as a parallel bit bus for A2D sampling through an external A2D device. The sampling resolution could be low as 4bits thus 4 pins could be used for data. The sampling rate should be 100Mhz so it will take...

deckhard by Associate III
  • 1849 Views
  • 3 replies
  • 0 kudos

Resolved! NUCLEO L432KC. How to print on TeraTerm using printf function?

Hi! My name is Vincenzo.I'm studying the board L432KC and I can't understand why using the HAL_UART_Transmit function I can transmit data on the terminal, while using the printf function nothing appears. Is there any preliminary operation to do? Than...

VNava by Associate III
  • 2444 Views
  • 3 replies
  • 0 kudos

Best way to interface external parallel ADC and DAC

Dear All,I have to develop a couple of boards: one to interface ADC LTC2202, 16 bits parallel, 10Msps and the other one to interface an external DAC AD5447, 12bits parallel, 10Msps.I will use for both boards STM32F429ZIT. My questions are:what is th...

Resolved! L031K6 : Please check my ADC-DMA code is correct !

I wish to get proper ADC value by ADC-DMA multi channels.These ADC-DMA has 4 channels : trying to get 3 voltage data from 3 external port , and temperature data from one internal port.but I realize I get quite incorrect value from external port ,and ...

DU2 by Associate II
  • 3427 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.