sd-card read write mode speed same in SD 1 bit mode and SD 4 bit mode?why
i m writing data in 1 bit mode or 4 bit both have the same speed, i m using stm32f746g discovery board. and what can be the max read write speed?
Ask questions, find answers, and share insights on STM32 products and their technical features.
i m writing data in 1 bit mode or 4 bit both have the same speed, i m using stm32f746g discovery board. and what can be the max read write speed?
I have the STM32G030K6T.Connecting a magnet to my magnet detector causes HAL_GPIO_EXTI_Rising_Callback and removing the magnet causes HAL_GPIO_EXTI_Falling_Callback. I think I have too much code inside these functions. Inside these functions I'm fadi...
Deleted post content, unable to delete due to administrative privileges.
Dear experts,I bought a MX25V8035F chip. I try to build my own SPI driver to communicate with this chip. I use STM32L071cb, STM32CubeIDE, and HAL Libraries right now. But, the STM32L071cb always receives a random number. for example, I try to read th...
Hi, thank you very much for the STM32G0 series, this really is very nice.Just for some applications I would need optioinally more CPU power, esepecially divide and best also floating point (so Cortex M3/M4 woudl be nice).I do NOT need higher speed / ...
#define STARTUP_MSG "Test Rx-interrupt\n" #include <stdio.h> #include "stm32f4xx_hal.h" #define get_RTC HAL_GetTick #define LED_inv HAL_GPIO_TogglePin(GPIOA,GPIO_PIN_5) #define LED_on HAL_GPIO_WritePin(GPIOA,GPIO_PIN_5,GPIO_PIN_SET) #define LED_o...
I'm using servo and driving it with servo motor. I want to print the servo degree via UART to serial. But im getting unknown characters. My code is;/* USER CODE BEGIN 0 */ uint32_t potadc; uint32_t servopot; /* USER CODE END 0 */ /* USER CODE BEGI...
The control tool can correctly identify the Imported IODD-file, but when i try to setup the IO-link communication in the control-tool I recieve the COMLOST fault. Furthermore I receive an Event error with the code: 49415. The STEVAL-IOM001V1 is corre...
I bought this kit to learn but after first time debugging i can't connect to it at all.I just set some GPIO input and outputs and got a led working in debug mode and now i can't connect to the board again and the previous debug program doesn't work e...
Hi,I am trying to learn how to use the LPTIM1 of the STM32L433 Nucleo-64 board (with the CPU: STM32L433RCTxP). I want to experiment on generating an interrupt every second with the LPTIM (I usually use a TIMx peripheral for this, but was interested b...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.