STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F051r8t6 SPI initialization issue

Hello.I'm trying to use SPI interface in STM32F051r8t6 micro on my STM32F0 discovery board. I got it to send data, but I set data lenght to 8bit, it is sending double that (first 8 is my data, but second 8 bit is always 0x00). When I set it to 4-bit,...

0693W000005A1GZQA0.jpg
fifi_22 by Associate III
  • 1381 Views
  • 1 replies
  • 0 kudos

SysClock to 216MHz on STM32F7 using PLL not working

Hi, I am trying to set SysClock to 216MHz using stm32f769xx.hI have no access to MCO pins, so for testing I am trying to blink a led every second. ARR and PSC values to achieve it will confirm if I am to desired SysClock frecuency (Blink led using ti...

RCres.1 by Associate III
  • 898 Views
  • 0 replies
  • 0 kudos

Send reset with DFU using Cubeprogrammer Api

Hello,I am using STM32 CubeProgrammer Api and I succesfully bootload my STM32H743ZI but it stays in bootloader mode after download, is there any way to ask a reset ?There is a reset function in the dll but it specify that it only works in SWD/JTAG mo...

Quadrature encoder interface timestamping

Hi,I'm using the STM32G474 in dual BLDC driver application.I'm operation the encoder interface at X4 mode. For RPM calculation I would like to time stamp every transition event i.e. encoder count + timestamp.Timers in use: TIM1/8 - PWM, TIM2/3 - hall...

heifetsg by Associate II
  • 763 Views
  • 0 replies
  • 0 kudos

Why CubeMX use so many memory? I create the blink test from Stepbystep on NUCLEO-L011 with default settings (UART disabled). When I compile the project, it takes 77% of RAM and 33% of Flash.

There is somthings wrong in settings of my CubeMX?There is some optimizzatione that I can do?If I don't use CubeMX ( and so I don't use HAL), there is another libraryes that I can use in order to manage the MCU without managing register ?Thanks.

ABatt.1 by Senior
  • 1218 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.