2020-10-30 11:37 AM
2020-10-30 1:14 PM
Check that each chip NACK to its slave address.
Check the error/status codes returned by the HAL_I2C functions.
You'll need to sequence your code such the it queries one at a time.
2020-11-01 3:31 AM
Ok ,.
Actually am using SPL and Not HAL.
Can you please share more on NACK to Slave Address? How to confirm it?
I am not much familiar to it.
Rohit
2020-11-01 4:46 AM
It is part of the I2C protocol, should be detected and flagged as part of the driver implementation.
If you are currently having an issue, see how the driver is reporting error/status conditions, and how you react to them.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.