Resolved! I purchased STM32F411 Discovery board but have not been able to download STSW-STM32080 DfuSe software for managing bootloaders.
The download attempt repeatedly fails and directs me to this site for help.
Ask questions, find answers, and share insights on STM32 products and their technical features.
The download attempt repeatedly fails and directs me to this site for help.
We are selecting a controller for our new Automotive project with CAN - FD connectivity, but we want to know whether ST provides the driver stack for CAN - FD for above microcontrollers for free.
I am using STM32 F767zi MC and I want to communicate with RS485 encoder. This is my code which has written in stm32f7xx_it.c. When executing this code, it can be seen that encoder and MC communicating continuously (observed using oscilloscope). But ...
HiI am planning to run a RAM test on STM32h743 RAM module. But I noticed that the RAM is divided into 3(SRAM 1,2,3) .Are these three RAMs physically different or the same RAM divided into three modules.Thanks in Advance
Hello everyone, this is my first post here. I am actually working on custom pcb with a STM32F410RB, which is used to count an external signal.To do this I use 2 timers, Timer 9 configured in internal clock and counting a 1 second period and generate ...
how to work on 16bit addressing in I2C.
Hello,I have a problem with with the HAL_QSPI_Receive() function:If I configure USB MSD on the device the code bellow does not work anymore. The code stops with an error at i = 64. Code work for exact 64 iterations. If I don't configure the USB-MassS...
I'm working on FDCAN & CAN interface provided on H745XI-DISCO board. I was new to these interface when I started, but now I can say I have good understanding on CAN & FDCAN Bus protocol. Using provided examples with STM32CubeIDE FW for H7 series, I w...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.