2020-09-10 12:03 AM
I'm working on FDCAN & CAN interface provided on H745XI-DISCO board. I was new to these interface when I started, but now I can say I have good understanding on CAN & FDCAN Bus protocol. Using provided examples with STM32CubeIDE FW for H7 series, I was able to achieve communication over CAN & FDCAN interface; on board between two CAN/FDCAN interface and also across the board using two different DISCO boards.
But now coming to the question, I was able to understand all the init parameter required for FDCAN handle except following 8...
This is configuration I have used from FW example, and I'm able communicate over CAN/FDCAN interface, but I'd like to understand these settings thoroughly, how it impacts CAN/FDCAN Bus.
hfdcan1.Init.NominalPrescaler = 0x1;
hfdcan1.Init.NominalSyncJumpWidth = 0x8;
hfdcan1.Init.NominalTimeSeg1 = 0x1F;
hfdcan1.Init.NominalTimeSeg2 = 0x8;
hfdcan1.Init.DataPrescaler = 0x1;
hfdcan1.Init.DataSyncJumpWidth = 0x4;
hfdcan1.Init.DataTimeSeg1 = 0x5;
hfdcan1.Init.DataTimeSeg2 = 0x4;
While searching for explaination/understanding I got to know that these are required for bit-rate settings of your CAN/FDCAN bus. But it is still unclear to me how Bit-rate & these parameters are related? How bit-rate is changed using fine-tuning of these params.
Any help is appreciated. Thank you!
2020-11-03 2:14 AM
Hello,
I hope this can help:
NominalPrescaler; < Specifies the value by which the oscillator frequency is divided for generating the nominal bit time quanta.
NominalSyncJumpWidth; < Specifies the maximum number of time quanta the FDCAN hardware is allowed to lengthen or shorten a bit to perform resynchronization.
NominalTimeSeg1; < Specifies the number of time quanta in Bit Segment 1.
NominalTimeSeg2; <Specifies the number of time quanta in Bit Segment 2.
DataPrescaler; < Specifies the value by which the oscillator frequency is divided for generating the data bit time quanta.
DataSyncJumpWidth; < Specifies the maximum number of time quanta the FDCAN hardware is allowed to lengthen or shorten a data bit to perform resynchronization.
DataTimeSeg1; < Specifies the number of time quanta in Data Bit Segment 1.
DataTimeSeg2; < Specifies the number of time quanta in Data Bit Segment 2.
For more informations you can check the RM0399 and the stm32h7xx_hal_fdcan.h file that you can find in the FDCAN exemple in the STM32Cube_FW_H7.
Br,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.