STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F415RG missing bytes on UART RX

Hi,I have a board containing an STM32F415RG and another board containing an MCU from another manufacturer. Both boards are supposed to communicate with each other using RS-232 transceivers. The communication is running at 9600 baud and working well f...

TSchm.1 by Associate II
  • 5108 Views
  • 6 replies
  • 0 kudos

PWM formula timer5 not work

I'm using STM32l152 and use TIM5_Ch2 for generate pwm .My target frquency pwm is 2.85 KHz .I using these parameter:clock frequency = 32MHz htim5.Init.Prescaler = 6;  htim5.Init.Period = 100; I measured pwm on oscilloscope and I measure 2.85KHz with 5...

bfran.1 by Associate II
  • 1604 Views
  • 3 replies
  • 0 kudos

STM32H745 and SPI + DMA

Hi to all,I need to send on every TIM interrupt a packet stream to SPI1. I can't use the HAL_SPI_Transmit(...) because it is blocking....so I need to use the DMA but not in circular mode.I can not use the synchronization of DMA with lptim using DMAMU...

DMast.1 by Associate II
  • 950 Views
  • 0 replies
  • 0 kudos

How to import Stmcube Mcu package examples code in atollic true studio? I want to run I2C communication between two nucleo STM32103RBx Boards How can I import it or I have to do it with STMCubeMx?

I have Run blinky code USART code with STMCUBEMx and atollic studio now I want to implement I2C communication between Nucleo boards. I searched And download stmcube MCU Package for STM32F1 series I have put it in the same workspace (same worksp...

DJosh.0 by Associate II
  • 692 Views
  • 0 replies
  • 0 kudos

sleep when pressing a button on keypad

My target is :my device when the main run is OFF = SLEEPThen its right this code ?When i pressed for a time > 300 mses button (OFF/on ) my device must wakeup , my button il connected to pin wakeup this is my code Which timer and i must use for t...

0693W000006G6VfQAK.png 0693W000006G6VaQAK.png
bfran.1 by Associate II
  • 725 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.