STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Stm32H750 FDCAN Interrupt lines confused

In the stm32H750 reference munal, I can see the details of fdcan interrupt, mostly by config registers (FDCAN_ILS, FDCAN_ILE ), but I didn't see the illustration about which interrupt signal(like tx complete ) occurs in which interrupt line(line ...

AresINSt by Associate
  • 1569 Views
  • 2 replies
  • 0 kudos

Resolved! Real-life UART with DMA using HAL ?

Hello,Is it possible to use uart with dma, so that on idle we also get informed, so that we can read the rx data ?I found no example in hal cube for using UART with DMA in such "real life" scenario, only in simple full buffer fill - which is not prac...

ranran by Senior II
  • 6633 Views
  • 9 replies
  • 1 kudos

There is a minor issue in pin names of STM32H750XB datasheet

Hi sir/madam,In the datasheet of STM32H750XB 57th page J1 pin name is given as PH0-OSC-OUT and in 61st page the same pin is given as PH1-OSC-OUT. which do we need to consider?Datasheet: https://www.st.com/resource/en/datasheet/stm32h750ib.pdf 

0693W000006Gj2DQAS.png
PY.1 by Associate II
  • 1279 Views
  • 2 replies
  • 1 kudos

Trying to integrate the waveplayer from stm32137 example in L4+ MCU. However, the loop updating the DMA buffer only enters DMATxComplete on 3 occasions?

Here's the essence of what I have at the moment. I wonder why it does not enter DMATxComplete, I have tried with 128 and 30 buffer sizes...//****** dac.c **********//   DAC_HandleTypeDef hdac1; DMA_HandleTypeDef hdma_dac_ch1; DMA_HandleTypeDef hdma_d...

VNado.1 by Associate III
  • 2451 Views
  • 4 replies
  • 0 kudos

DAC output error

I'm using STM32F405VGT6 to output sine wave by using its dac.After every output sample,which is triggerd by timer, dac's data holding register 'DAC_DHR12R2' is not holding the data and is reset to zero.So the output wave is something like sine wave m...

ZPC.1 by Associate
  • 1126 Views
  • 1 replies
  • 0 kudos

wrong data send with slave i2c1 on STM32F103RCT6

STM32F103RCT6 i2c work as slave mode,master i2c machine worked with clock speed 400KHz.When master read many bytes from slave,a wrong data will come out behind the address byte.in normal,master transmits 0xA1,then it will receive 0x11 0x22 0x33 0x44b...

yqiu.11 by Associate
  • 1224 Views
  • 1 replies
  • 0 kudos

EXTI line got odd/even interrupts count.

Hi friends,I met a problem.I used one EXTI line to check a button push-and-release. EXTI line was set to be triggered by both falling and raising edge. I know there will be burr when I pushed the bottom. The question is , when I pushed and then relea...

EYang.11 by Associate II
  • 1331 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.