STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f7 RTC clock waveform is very small

The external RTC clock of stm32f765igt6 chip, the waveform of the clock is very small, RTC clock is very inaccurate. This is whether the crystal oscillator or capacitor selection problem, or our single-chip RTC drive problem; For the external RTC clo...

晓杨.1 by Associate
  • 1268 Views
  • 1 replies
  • 0 kudos

LPTIM CFGR WAVEPOL description

Hello,both STM32L4 and G4 reference describe in LPTIM->CFGRBit 21 WAVPOL: Waveform shape polarity       The WAVEPOL bit controls the output polarity       0: The LPTIM output reflects the compare results between LPTIM_ARR and LPTIM_CMP  registersThis...

How STM32H747 dual-core M4 and M7 go into stop mode separately with the allocated peripheral DeInit and ReInit after wake up

Hi,I want to set the dual-core MCU into stop mode respectively with allocated peripheral like UART/ADC/I2C/SPI/TIMER, DeInit the peripheral and disable the corresponding clock and start a lptimer to wake up the core before entering the stop mode, lpt...

Vzhan.1 by Associate
  • 1001 Views
  • 0 replies
  • 0 kudos

Auto WakeUp due to floating of wakeup pins?

We are trying to build MCU application that require wakeup from standby mode using wakeup pins. MCU we are using STM32L412KB and it consists of 2 wakeup pins on PA0 and PA2.As per figure 3 we want to connect PA2 wakeup pin to USB V sense to wakeup us...

JKSah by Associate II
  • 4127 Views
  • 6 replies
  • 0 kudos

I2C slave is not working in reading and writing

I am using STM32F7508-DK kit and Using I2C as a slave whereas ESP32 is a master, By using HAL_I2C_Slave_Receive_IT and HAL_I2C_Slave_Transmit_IT API I am able to do one way communication either read or write, but in my application I required read and...

Is there a difference in startup time between STM32F303 and STM32F407? I am experiencing relatively longer start up time for the STM32F407..

I refer to the attachment. I am using a push button to power on a STM32F303. As soon as the push button is pushed a P channel FET is activated supplying voltage to the STM32F303. As soon as the STM32 starts it activates a pin which takes over activat...

MBooi.1 by Associate II
  • 1978 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.