STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hello All, I am facing following problem while working with STM32L4R5 MCU. Can you please give why this problem occurs? What will be solution for this? Please explain step by step process to resolve this issues.

11:42:17 **** Programming project stm32l4xx_drivers on chip ****"C:\\Ac6\\SystemWorkbench\\plugins\\fr.ac6.mcu.externaltools.openocd.win32_1.23.0.201904120827\\tools\\openocd\\bin\\openocd.exe" -f stm32.flash.1849521082279362012.cfg -s "C:\\Users\\Hi...

PPran.1 by Associate
  • 1215 Views
  • 1 replies
  • 0 kudos

BOOT probem

I have working with STM32L083... Since now no problem observed but my last pcb has BOOT problem... Namely when I ACTIVATE BOOT signal STM enter to boot mode but when I relesed taster for boot signal MCU resume from boot mode... earlier version of pcb...

MJova.1 by Associate II
  • 1218 Views
  • 1 replies
  • 0 kudos

Output compare to turn on a LED

Hello,I am working on a STM32F723E-Disco,I am learning the use of timers and their functionalities.In particular, I try to use the output compare.What I'm trying to do is to use the output compare to turn on a LED when the output compare is triggered...

SGROU.1 by Associate III
  • 2584 Views
  • 5 replies
  • 0 kudos

I want to mak a decoder input signal by counting 25Mhz clock. The 25Mhz clock signal should also come out to the output port.

Set the APB2 timer to 180MHz to generate a 25MHz clock signal in output compare mode.And it tries to increase the decoder signal by 1 by counting every 513 rising edges.However, the decoder input signal is toggled on more than 513 signals.By changing...

선권.1 by Associate
  • 1909 Views
  • 2 replies
  • 0 kudos

I am using STM32CubeMX to generate an MDK-ARM project for NUCLEO-L552ZE-Q. If, in the clock configuration tab, I select HCLK/8 as SysTick clock source, the SysTick initialization code generated produces a wrong time base.

The problem arises because by selecting both HCLK and HCLK/8 the SysTick is always initialized like this:SysTick->CTRL = SysTick_CTRL_CLKSOURCE_Msk | SysTick_CTRL_ENABLE_Msk;thus selecting HCLK as clock source in both cases.Maybe the correct code sh...

GRizz.1 by Associate
  • 634 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.