STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L452RE Read Out Protection at random time

Hi,we have a problem with low power application developed on STM32L452RE with BLE BlueNRG-M2SA module to read environmental sensors (STTS751, HTS221 and LPS25)The application is developed on the STM32CubeIDE (1.5.1)At the start of main code the IWDG_...

AColino by Associate
  • 951 Views
  • 1 replies
  • 0 kudos

Resolved! SAI in SAI_I2S_STANDARD Mode...

What happened to the equivalent of I2S_FLAG_CHSIDE as I don't seem to be able to find it.Or do you just count the interrupts and assume it goes Left - Right - Left... forever?ThanksAndy.

Resolved! STM32H743ZI I2C4 unexpected interruption

Hi,I recently need to use I2C with interrupt mode to lower my CPU usage.So I did this changes :I changed the function where I call my transmitstatic HAL_StatusTypeDef PGA309_Write_RawData(uint8_t REGISTER,uint8_t LSB_DATA,uint8_t MSB_DATA) { uint16_...

LSI in Backup Domain on STM32H735.

Datasheet and Reference Manual have contradictions about the LSI Power.Information from Datasheet:The RTC is functional in VBAT mode and in all low-power modes when it is clocked by theLSE. When clocked by the LSI, the RTC is not functional in VBAT m...

0693W000007DDJyQAO.png
DDuque by Associate
  • 2291 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.