STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Error occurs when HAL_PWREx_EnableOverDrive() is executed.

clock configurationMCU: STM32F767IITIDE/Debugger: STM32CubeIDE / SEGGER J-Link​When HAL_PWREx_EnableOverDrive() is executed after changing the block size of SPI Flash, the following error occurs: Break at address "0x64da2200" with no debug informatio...

0693W000007EGHdQAO.jpg
pabian by Associate III
  • 1010 Views
  • 0 replies
  • 0 kudos

Can DMA output a byte stream with 8080 style 'write' strobe?

Hi everybody,I am using STM32F401CE and would like to use DMA to output a block of bytes using a 8 bit output port and a 'write' strobe output. That is, 8 output pins + 1 strobe output for the strobe pulse, per the timing diagram of the ILI9341 TFT s...

JSmit.18 by Associate II
  • 2645 Views
  • 5 replies
  • 0 kudos

ST now charge for material for workshop

I remember ST use to provide workshop and material(boards) for free in order to attract professional to experience their product. Now on top of all the difficulties some of us experience they charge the full price with a a small discount for shipping...

Low power mode oscillator

Hey,in my application, ill have an RTC function, that should work also when power in down.From this reason, I’ll use a battery that will be connected to VBAT pin.My question is about LSE clock.my plan was to connect an external oscillator 32.768kHz t...

Pkats.1 by Associate II
  • 1903 Views
  • 2 replies
  • 0 kudos

Resolved! GPIO pins stuck in HIGH state

HiI am working on a project using LL libraries and STM32F407VET6 Board. (I have attached the main.c code here.) The code generated by the STMCube GUI configuration tool is causing issues with two GPIOA pins (Pin 6 and 7) stuck to HIGH whenever the co...

MVerm.2 by Associate III
  • 2461 Views
  • 2 replies
  • 0 kudos

Resolved! STM32G474 HAL_TIM_Encoder_Start_DMA Question

Hello STM32 MCU Community,I was looking for clarification on the HAL_TIM_Encoder_Start_DMA function as I want to do a DMA transfer of an encoder's count register to a buffer. From the STM32G474 reference manual, I thought I would need to use another ...

KKerr.2 by Associate II
  • 4678 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.