STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Where I can find patch for STM32Cube_FW_F4_V1.25.2 firmware?

Hello,My problem is similar to this one: https://stackoverflow.com/questions/65905606/stm32cubeide-reports-firmware-package-is-missingUnfortunately I cannot find the patch they were talking about (Patch-CubeF4). After going to the following site: htt...

MJaks.2 by Associate
  • 1414 Views
  • 1 replies
  • 0 kudos

Setting core affinity or switching between cores in STM32H757

Hello Team , Setting core affinity or switching between cores in STM32H757,We are in early phase of design and looking to go with STM32H757XI , We are still not sure which thread to be run on which core ( M4 or M7) We are looking to use keil rtx5 CMS...

CMatad by Associate II
  • 1436 Views
  • 4 replies
  • 0 kudos
TPati.2 by Associate
  • 1512 Views
  • 1 replies
  • 1 kudos

Unable to flash STM32H7B3I-DK

I have tried flashing from TouchGFX and also from CUBEIDE. I did manage to run a first trial of example but after the 3rd modification is went black.The lcd remains black. I add a screenshot with the log from TouchGFX . It states failed to erase memo...

0693W000008wstcQAA.png
BHure.1 by Associate III
  • 702 Views
  • 0 replies
  • 0 kudos

STM32G070 HAL_UART_ErrorCallback

Dear all,I have 2 MODBUS 485 ports, one in UART1, the another in UART3, both in DMA mode.Testing frame collisions with Docklight I see the function HAL_UART_ErrorCallback called with an Error code of 1 (Parity error), 8(Overrin error) or 11 (Parity+N...

0693W000008wdEzQAI.png
DPrie.1 by Associate II
  • 5925 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.