STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to enable Data Length Extension with BlueNRG-MS

BlueNRG-MS claims to support the Bluetooth Core Specification 4.2, which includes the data length extension. However, I don't find any pointers on how to enable it. For the BlueNRG-2, there appear to be special commands in the HCI LE API (see https:/...

ADusc.1 by Associate
  • 992 Views
  • 0 replies
  • 0 kudos

Video from USB camera to TouchGFX

I have a USB camera connected to a STMF746G Discovery board. I like to get the frames from the camera and show them in a TouchGFX application (e.g. using dynamic bitmaps). How do I get the camera frames? Is there any simple code example?

diewet by Associate
  • 585 Views
  • 0 replies
  • 0 kudos

Pin slew rate setting of STM32F746

Hello,GPIO port output has a speed register (GPIOx_OSPEEDR).When I use it for functions other than GPIO, can I set the slew rate with this register?If not, is there any other way to set the slew rate?Goto

Resolved! STM32F407 Uart Byte Received error(higher4bit)

Hi,​Using "STM32F4xx_DSP_StdPeriph_Lib_V1.8.0" to config STM32F407 Uart1 as following​///////////////////////////////////////////////////////////////////////////void USART1_Init(u32 baudrate){​ USART_InitTypeDef USART_InitStructure; GPIO_InitTypeDef ...

0693W000008x1SVQAY.png 0693W000008x1R3QAI.png 0693W000008x1TEQAY.png
jhl14 by Associate II
  • 1140 Views
  • 1 replies
  • 0 kudos

Resolved! Can STM32H743 (With TIM1/TIM8) control two 3-ph Inverters?

Hi everyone,Thanks in advance for your time.Im starting my first application in ST: a power converter controller. I need to be able to control two three-phase inverters with SPWM modulation, for which I think STM32H743 is the microcontroller I need. ...

Yvo by Associate II
  • 4109 Views
  • 10 replies
  • 0 kudos

Assistance with Debugger Issue

Hi all, I've been battling a frustrating issue on my STM32F407 Discovery board for the past few days. I don't know where the fault lies exactly but hopefully if I explain someone can point it out. I'm working on a robotics project, not doing anything...

GEvan.1 by Associate
  • 1379 Views
  • 1 replies
  • 1 kudos

1GB memory usage instead of 512MB for STM32L4R9AI

The STM32L4R9AI documentation says that it supports Macronix MX25LM51245GXDI00 and Micron MT35XL512ABA1G12-0SIT Octo-SPI Flash memories. These modules are not currently available for sale.Please tell me, is it possible to use MX66LM1G45GXDI00 instead...

VTeli.2 by Associate II
  • 6986 Views
  • 5 replies
  • 0 kudos

QSPI issue

I am using STM32F746 controller and MX25L128 flash on a custom board.I want to make external flash loader file for my custom board.I followed the MOOC - External QSPI loader how toI got error while memcmp for (var = 0; var < SECTORS_COUNT; var++) { ...

NMait.1 by Associate II
  • 1114 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.