STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Supplying voltage on VBAT pin on STM32F469I-DISCO

Hi everyone, I am currently working on a project working on a STM32F469I-DISCO. I would like to be able to use the embedded RTC as well as the backup SRAM. I have seen on the schematic that the VBAT pin is tied up to the 3.3V. Is there a way to still...

NKieg.1 by Associate III
  • 3009 Views
  • 7 replies
  • 0 kudos

Discrepancy chip marking vs product/chip ID ? My chip marked STM32F100V8T6B give a productID 0x414, while I expected 0x420. Have I received a batch of chips with an incorrect marking?

According to AN2606 rev 14, pid 0x414 mean high-density device, pid 0x420 mean medium-density device. We just bought 500 STM32F100V8T6B. They are deployed in an existing modular product that programs the uC in-situ. The program relies on the PID to ...

BNoss.1 by Associate II
  • 8449 Views
  • 15 replies
  • 0 kudos

STM32F072-EVAL- In this I am using given UART Example with Board in STM32Cube_FW_F0_V1.11.0 firmware. I am using RealTerm to check UART communication. ON Real Term I am receiving Garbage Character, I tried by changing baud rate but no correct response.

STM32F072-EVAL- In this I am using given UART Example with Board in STM32Cube_FW_F0_V1.11.0 firmware.I am using RealTerm to check UART communication.ON Real Term I am receiving Garbage Character, I tried by changing baud rate but no correct response.

SDwiv.1 by Associate II
  • 1642 Views
  • 1 replies
  • 0 kudos

Resolved! What should I do If I don't have the same version of tools?

I have STM32CubeIDE, STM32CubeMonitor and STM32Cube_FW_H7 ,but they are not the same version as the required version.Some are older version and some are newer versionWhat should I do.1-Should I uninstall my already installed SW and use the "STM32H72x...

HAlzo by Senior
  • 1037 Views
  • 1 replies
  • 0 kudos

SAI FS configuration

Hi,I have a design that uses a STM32H757 with an external ADC that streams data out to the SAI peripheral. The ADC is the bus master and generates the clock. The ADC data is the PCM / DSP protocol format.I setup my SAI with the free protocol configur...

0693W000008xDszQAE.jpg
TMiha by Associate II
  • 2662 Views
  • 3 replies
  • 0 kudos

STM32H7 ADC12 and ADC3 noise discrepancy

Hello everybody,I need to acquire a signal at about 4MS and want to use the ADC1 and ADC2 of an STM32H7 (rev V).In a previous project, I only had direct channels of ADC3 available on the package.Hence, I compared my measurements to ADC3.Unfourtunatel...

Board dumping problem

Recently we have purchased STM32NUCLEO-H7A3ZI-Q Nucleo board for our application development.Whenever we are trying to dump the code into board,we are facing error and attachment is attached for the same.We have tried with pulling the boot up pin as ...

Chethan by Associate II
  • 1845 Views
  • 4 replies
  • 0 kudos

CAN NORMAL MODE WITH TWO STM32f407 discovery kit?

Hello everyone, i am new to approaching st boards.My goal is to create a Can BUS communication between two stm32f407 discovery boards (normal mode).I initially approached can using the loopback mode example.Now I wanted to move on to the next step by...

Apicc.1 by Associate
  • 2163 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.