STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Why can I only use 2 GPIO pins?

I am only able to use 2 GPIO pins with an STM32F767ZI on a Nucleo-144 board. The issue doesn't appear to be with any specific pins, it's just that only 2 pins seem to output any voltage at all.Take this code for example:main.c#include "./headers/stm3...

Starman by Associate II
  • 6165 Views
  • 23 replies
  • 0 kudos

Wire Bond Lengths Inside BGA

I am working with the stm32f407igh6 and need to account for timing in my layout. I have been unable to find documentation regarding the wire bond lengths inside the BGA. Are all the line lengths in side tis BGA the same length?

LWood.2 by Associate
  • 1296 Views
  • 1 replies
  • 0 kudos

BPSK unmodulation only with STM32

hello all, for an internship I work on modulation / unmodulation BPSK.For the modulation I used a DDS drive by a stm32.But I want to know if it's possible to make the unmodulation only with STM32. I know we can measure the freq with it but can it do ...

Seth1er by Associate II
  • 1054 Views
  • 0 replies
  • 0 kudos

Board-To-Board abstraction protocol (MUX, eRPC..)

Hi FolksI'm running a design where i have a sort "Expansions" board where all the Analog inputs and RS485 / UARTS port are located.This board is running a STM32F107 mcu.Then i have another board running a STM32F429NIH6 MCU, where we handle LCDs, ETH...

Hard fault for unknown reason

Hello,this is my functionvoid process_dds_ext_demod(uint16_t *inbufPtr1, uint16_t *inbufPtr2, float *in_phase_val, float *quadrature_val){ /*transfer DMA buffers to local Buffers-------------------*/ //transform values from int to float float ADC1_Bu...

HBesi.1 by Associate II
  • 1215 Views
  • 1 replies
  • 0 kudos

STM32F7 SAI SPDIF TX channel status / frame count

Dear STM32-SPDIF-TX experts,I'm working with a STM32F767 on a Nucleo-144 board.Creating a sine, sending data at 24bit/192kHz via DMA / SAI 2B, everything fine.Filling the output buffer for SPDIF within the HAL_SAI_TxHalfCpltCallback() & HAL_SAI_TxCpl...

LCE by Principal II
  • 1314 Views
  • 1 replies
  • 0 kudos

stm32G474 adc ground offset

Hello,I am having an issue with an offset on my ADC measurements. I am using the NUCLEO-G474RE, and I am using pin PA8 as the analogue input.When I measure an analogue pin, the value measured is a bit higher than the actual values. (Actual values mea...

Azeve.1 by Associate
  • 2604 Views
  • 1 replies
  • 0 kudos

STM32G4 Flash writes at BOR

Hello,We have currently moved on to the STM32G4 series, and we are now looking at a project where data will be occasionally written to flash under control of our own code. Of course, this exposes us to flash memory corruption during unforeseen power ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.