STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem Using Jump_To_Application() in app programming (IAP)

Hello there.I'm using a stm32F417VGT6 to perform an IAP in Keil IDE.in the bootloader, using the Bin file on a SD card, I read executed Binary program and write it on flash memory. then i use  Jump_To_Application() to start the new app. Everything wo...

Seyed by Associate III
  • 1476 Views
  • 2 replies
  • 0 kudos

STM32F7 SPI TxFIFO problem

Hi!I have a SPI master that communicates in the following way:CS is setStart sending data in the following format - 2 bytes of "request"2 bytes of crc for the "request"x bytes to clock out the response from the slaveCS is releasedOn the slave side (S...

Does anyone has experiment project to erase and write to Parallel flash . We connected 16 Mega Bytes Parallel FLASH Chip and we are Using FMC interface on STM32H745XI .

Does anyone has experiment project to erase and write to Parallel flash .We connected 16 Mega Bytes Parallel FLASH Chip and we are Using FMC interface on STM32H745XI . Following driver is being used but I could not find and example project to write t...

Binary compatibility between F091 and G0B1 series

Due to dwindling stock levels we need to migrate from a F091 to a G0B1 series microcontroller. To keep compatibility for devices in field(for future firmware upgrades) I was wondering if it was possible to run the same code binary between the two mic...

ABish.1 by Associate
  • 1245 Views
  • 1 replies
  • 0 kudos

Need help for CSS on STM32H7 in power-optimized designs

Suggest a STM32H7 running from external clock source on HSE input. CSS is enabled. HSI is disabled due to power consumption issues.What happens if HSE fails?Will CSS start the HSI oscillator before switching to HSI clock source?Thanks for your help!

Mat_ by Associate
  • 765 Views
  • 0 replies
  • 0 kudos

Resolved! What happens to a DMA trigger while DMA is not enabled?

Hello,I couldn't find anything about this in reference manual:I have configured TIM8 to generate a DMA request on update. When I set TIM8, register EGR, bit UG to force an update while both the timer and DMA are not enabled, what happens to the gener...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.