STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to boot the STM3241G-EVAL?

As shown in below my kit screen is completely white, is not able to see any menu?I have searched to how to boot the kit from STM website, I found a video and an document I want to do the same process, during doing the same procedure I am getting the...

0693W000001rmk2QAA.jpg 0693W000001rmkvQAA.jpg
HNory.1 by Associate
  • 1436 Views
  • 1 replies
  • 0 kudos

Dealing with CAN bus initialisation error (INAK)

Hi all:I have a bare-metal firmware running on an STM32F407VGT6, and I am implementing a CAN bus interface. It is a very simple "slave" device that responds to short commands.Most basic CAN bus operations are working, but I still haven't finished the...

Diez.R. by Associate II
  • 3144 Views
  • 0 replies
  • 0 kudos

STM32L011 RAM usage

Hello,I am using STM32L011 MCU and STM32CubeIDE environment. After generating project with CubeMX and even deleting initializations in main function, 'Build analyzer' section shows that 76 % of RAM memory (of total 2KB) is used. What might consume so...

Indois by Associate II
  • 1708 Views
  • 2 replies
  • 0 kudos

Is there a way to export all the settings used in the STM32CubeProgrammer GUI, once here I succeded flashing my MCU?

Hello everyone,I installed the STM32CubeProgrammer v2.6.0 for ubuntu and I was able to use the GUI to flash a binary file into the MCU (NUCLEO-G431RB).My aim is to write a shell script to execute this task, therefore my question....Thanks in advance ...

DCasa.3 by Associate
  • 1208 Views
  • 1 replies
  • 1 kudos

DMAMUX Synchronization trigger only once

I have working sytem with 4 ADC and 4 DMASince Im triggering 2 ADC with one Timer (at fixed 25 kHz) and 2 ADC with another timer (at variable 70-240khz) I want to synchronize the DMA data from all ADCs (to the frequency of slower 25kHz timer)So in on...

KoRba88 by Associate III
  • 1258 Views
  • 1 replies
  • 0 kudos

Resolved! Use Analog Watchdog (ADC AWD) as a reset for timer.

I've to count till 30ms, but i've to restart the count if a signal goes above a threshold. So i want to use analog watchdog as trigger source for the timer. I set up the timer in "slave reset mode" and with "ETR1 through ADC" as Trigger Source. I've ...

MPian.1 by Associate II
  • 4700 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.