STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Use timer base and input capture at the same time

I use timer gated mode for a HC-SR04 ultrasonic sensor which needs microsecond delay. Is it possible to use the same timer as time base to get microseconds? if (HAL_TIM_Base_Start(&htim3) != HAL_OK) // time base for usDelay() Error_Handler(); if ...

Yuan1 by Associate II
  • 2799 Views
  • 5 replies
  • 0 kudos

Development IDE and tool chain details for EVLKST8500GH868?

We are considering EVLKST8500GH868-ST8500 Hybrid PLC&RF connectivity development kit for our plc development.It comes with Nucleo-G070RB please let me know development IDE and its toolchain needed for the development and also please mention license c...

Kkanu.1 by Associate
  • 610 Views
  • 0 replies
  • 0 kudos

STM103VET6 IS A GOOD IC OR NOT.

STM103VET6 IS A GOOD IC OR NOT. We can only set the pll to 48MHz , AND THE CAN function IS NOT ANY SIGNAL.WE CAN USE THE OTHER IC STM32V103ZET6 TO SET PLL TO 72MHZ AND THE CAN FUNCTION IS OK.SO, WE THINK THAT THE IC IS NOT GOOD , OR REMARKED IC.

0693W00000BaZzUQAV.jpg 0693W00000BaZzKQAV.jpg
Lgang.1 by Associate
  • 1179 Views
  • 1 replies
  • 0 kudos

BLE characteristic notification issues

Hi guys,I have two characteristics, one for get values from mobile applicationand the second one is to reply as notification to user, to the mobile application.I registered to notification characteristic, to reply the user for any changes.I have two ...

Lmali.1 by Associate III
  • 1307 Views
  • 1 replies
  • 0 kudos

2 lpuarts can't communicate to each other correctly

A board with STM32L071CBT6 and another with STM32L476RGT6. The former transmit 18 bytes data {02 6E 9B 3B 41 41 00 00 E7 41 96 83 C9 42 00 03 24 97} to the latter. the latter received {02 6E 9B 3B 41 41 00 00 E7 41 96 83 D9 42 00 03 24 97}, that's t...

JZhen.6 by Associate
  • 1674 Views
  • 3 replies
  • 0 kudos

STM32F103C8 ADC internal temperature read way too high.

HiUsing the STM32F103C8 with STM32CubeIDE and bare metal programming, I am trying to read the internal temperature. While I manage to read the ADC, enter the ADC ISR and do the calculation to get the temperature, the result is unrealistic. The data r...

AAnth.1 by Senior
  • 5042 Views
  • 6 replies
  • 0 kudos

fast adc calculation

I am using 46uSec sample rate adc to acquire 6 channels data using adc time to trigger adc with dma transfer, but I would like to do average every 4 samples, and do some other calculation every 30 samples. I use 3 channels in Timer 4 to realize adc t...

yang hong by Associate III
  • 1205 Views
  • 2 replies
  • 0 kudos

Does NUCLEO-L4R5ZI-P board support Hyperbus Protocol?

I saw that Hyperbus protocol with differential clock (1.8V) is not available on STM3L4R5ZIT6P, but Hyperbus protocol with single-ended clock(3.3V) is. My question is : is the Nucleo -L4R5ZI-P board supporting Hyperbus protocol with single-ended clock...

AGEBE.1 by Associate II
  • 1183 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.