STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to configure HRTIM in Up-Down Counting Mode

I am using STM32 G474RE with STM32CubeIDE 1.6.1 with HAL configurations. I would like to use HRTIM1: Timer A with TA1 and TA2 enabled. My goal is to control TA1 PWM on the Up counting of Center Aligned counting (up-down counting), and control TA2 PWM...

0693W00000BbapmQAB.jpg 0693W00000BbaqVQAR.jpg 0693W00000BafcMQAR.jpg 0693W00000Bbar4QAB.jpg
CWatt.1 by Associate
  • 2227 Views
  • 0 replies
  • 0 kudos

Uploading to target devkit error. I have 2 x STM32F769 Discovery Kit. in 1 kit it's always running without any problem. in another kit most of the time I'm getting this error while uploading.

Run Target  Generate    Done  Generate Assets    make -f simulator/gcc/Makefile assets -j8    Reading ./application.config    Done  Post Generate    touchgfx update_project --project-file=simulator/msvs/Application.vcxproj    Done  Post Generate Targ...

RMuru.1 by Associate II
  • 870 Views
  • 0 replies
  • 0 kudos

Nucleo-h745ziq spi 1 and spi 3 MOSI pin mapping issue.

Hello ,I am using NUCLEO-H745ziq board. I am trying to loopbacking. SPI1 and SPI3 i am using. SPI1 as full duplex slave and SPI3 as full duplex master.Both operating on 25MHZ.But i have issue with is MOSI pin.Because PB5 is assigned to both. But when...

0693W00000BbUhNQAV.png 0693W00000BbUhcQAF.png
MDeva.1 by Associate II
  • 874 Views
  • 1 replies
  • 0 kudos

STM32 built-in flash endurance test, targeting STM32L4R7.

Good day.Lately, I had carried out a STM32 built-in flash endurance test, targeting STM32L4R7.I selected a sector which is : Bank 2, 0x081F F000 - 0x081F FFFF, 4K, page 255to perform erase and program, with the hope that it could eventually fail. So ...

Msee by Associate
  • 1207 Views
  • 1 replies
  • 2 kudos

Migrating from L4 to F4

What are the main points which I have to consider when migrating from STM32L4 to Stm32F4 apart from the connecting peripheral power management, Is there any main points which I have to consider when programming.

Roshan by Associate III
  • 2203 Views
  • 4 replies
  • 0 kudos

What's the difference between STM32L4S5ZI and STM32L496RET?

Hello, I just wanted to ask is there a big difference between STM32L496RE and STM32L4S5ZI. Other than STM32L4S5ZI having a larger RAM and memory. As well as no display interface but with encryption. I'm asking because the STM32L496RE is now out of st...

HAhme.1 by Associate II
  • 1680 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.