STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H74A3: How can I switch SPI Mode for 2 SPI-Slaves on the fly

I have a system with an STM32H74A3, which uses one SPI port for different slaves which use different SPI modes.One Slave needs Mode 3 (Pol.High/2ndEdge) and 8 Bit Data size, the other needs Mode 0 (Pol.Low/1stEdge) and 16 Bit. Clock Speed is the same...

GS1 by Senior III
  • 1978 Views
  • 2 replies
  • 0 kudos

BCM4 boot option byte, software modification on STM32H747

Hi, I am curently working on the STM32H747. I need to have the CM7 booting while the CM4 is not. Then after, the CM4 BOOT is triggered by the CM7.Using STM32 cube programmer, I am able to disable the BCM4 bit of the SYSCFG_UR1 register.The required s...

baptor by Associate III
  • 1991 Views
  • 2 replies
  • 0 kudos

Not able to update internal RTC in STM32F373

Hi,           I made a project for only internal RTC. It worked with LSI and not with LSE. Then I integrated RTC in current project which has various other features. It is not working. I am getting zero readings.      RTC initialization, get tim...

Ralph1 by Associate
  • 1851 Views
  • 3 replies
  • 0 kudos

No device found on target ERROR

I have a STM32NUCLEOF411RE. It was working well until today. Now my pc can not recognize it. It says "No device found on target.". Also when I connect my board the processor becomes too hot in a few seconds. However, when power it with 5V it does not...

AYelb.1 by Associate
  • 2707 Views
  • 5 replies
  • 0 kudos

Issue in STANDBY Mode in stm32f746g discovery board.

Hi everyone,I am trying to implement the STANDBY mode in stm32f746g board using the system wakeup pin PI11 (user push button). The issue is that once I press the button, the controller automatically wakes up from the STANDBY mode.I have attached my c...

SGupt.7 by Associate II
  • 1801 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.