STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F429 Discovery Kit LEDs does not blink

Dear STM Community,I am a Fresh learner of STM32 technologies. I got myself an STM32F429 Discovery Kit.As expected, I tried to do Led Blinks on my board since it is the hello world of this technology.However, I couldn't turn on the LEDs on board. I c...

0693W00000BdPLVQA3.jpg 0693W00000BdPLaQAN.jpg 0693W00000BdPLfQAN.jpg 0693W00000BdPPSQA3.jpg
SKAŞ.1 by Associate II
  • 2008 Views
  • 2 replies
  • 0 kudos

What is out put data rate of lis2dh and lis3mdl ?

i read data sheet of lis2dh and lis3mdl. i am using st linux driver to read raw data of accelerometer and magnetometer. Now when i set sampling frequency 1600 for accelerometer i get data of x axis at 40 ms. when i set sampling frequency 80 for ma...

Mpraj.19 by Associate II
  • 935 Views
  • 0 replies
  • 0 kudos

USART1_IRQ HANDLER ISR is not getting executing after enabling RXNEIE is set in cr1 and setting priority in NVIC_ISER1 register in stm32f401re nucleo board.anyinputs?

#include<main.h> #include<stdarg.h> void SystemInit(); void Uart1_config(); void uart_printf(const char *fmt, ...); void delay(int val); void Gpio_Enable(); void USART1_IRQHandler() { uint16_t rx; rx=USART1->DR; GPIOB->ODR ^=1<<3; USART1->...

Nchun.1 by Senior
  • 1635 Views
  • 4 replies
  • 0 kudos

Can't see the data using DMA and ADC

I'm using STM32F303RE, and I'm trying to sense analog values from different ports of the ADC using the DMA, but at the moment the application is running, I don't get any data. I tried to put an interrupt routine to see if the DMA is at least been cal...

I am having problems with QSPI interface here to talk to a 4Mbit NOR Flash (Flash MX25V4035F ). It looks like Initialization succeeds and chip erases. However, I get HAL error on sending any command such as Write Enable or Read ID.

The Hardware Configuration is /* Initialize QSPI Lines  *  * GPIO Pin Function * PE7  :  QSPI_BK2_IO3 * PFE8  :  QSPI_BK2_IO2 * PE9  :  QSPI_BK2_IO1 *  PE10  :  QSPI_BK2_IO0 *  PA7  :  QSPI_CLK * PC12  : QSPI_BK2_NCS  * */  GPIO_InitStruct.Pin =...

PRama.3 by Associate II
  • 5771 Views
  • 9 replies
  • 0 kudos

Resolved! STM32H7 CAN bus not receiving a particular unlucky message

I have a CAN bus between STM32H745 and STM32F042 processors using Standard CAN for communicating. The transfer, receive just works fine for any packet other than the following: I cannot explain it. The data byte starts with 0xd2 0x01, STM32H7 does no...

0693W00000BaZinQAF.png
hsamurai by Associate II
  • 3420 Views
  • 6 replies
  • 0 kudos

Resolved! What is the flash memory map for the stm32f205re and rf?

We are using the stm32f205rgt6tr. At present they are not available. We are looking at using the stm32f205re or rf as a replacement, but the memory map in the reference manual and flash programmer manual only have the map for the rg.

JDavi.9 by Associate
  • 1417 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.