STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is ST out of MCU business?

I cant seem to find any source for STM32 MCUs in any significant quantity. It seems ST stopped production and I find no evidence it will get better soon. Developing on STM32 platform seems like betting on a dead horse. Are we the only ones struggling...

snigg by Associate III
  • 2198 Views
  • 4 replies
  • 0 kudos

Resolved! STM32CubeMX STM32F4 Library Install Problem

Posted on January 24, 2017 at 19:55Hello all, I am running into a problem with updating the STM32F4 library in STM32CubeMX ver 4.19. I want to install the STM32F4 library package ver 4.14. However, I get an error stating 'These Files have problem du...

i have written a led blinking program with as per my knowledge but i couldn't reach output so guys who can clear that? MCU- STM32f401 clock input -25MHz External clock output -80 MHz with pll configuration

#include "stm32f4xx.h"#define PLLM 25#define PLLN 320#define PLLP 1//divide 4void SysConfigure(){      RCC->CR|=RCC_CR_HSEON;//External Crystal Oscillator      while(!(RCC->CR & RCC_CR_HSERDY));// External Crystal oscillator status flag checking     ...

Msams.1 by Associate II
  • 3045 Views
  • 7 replies
  • 0 kudos

Generating 1 nanosecond update event using Timers - AN4013

According to AN4013 on using timers as time base generators, one could use a 16-bit timer to generate an update event from a nanosecond to a few minutes. Well, take for example the STM32F429 clocked @ 180 MHz. If one cycle takes 5.56 ns, which is the...

0693W00000D0FIqQAN.jpg
Zaher by Senior II
  • 5959 Views
  • 10 replies
  • 0 kudos

Modbus over RS485 with STM32F303K8

I'm looking to make a loop of MCUs as slaves to a PC master so that I can send commands to them. The idea is to use the https://www.maximintegrated.com/en/products/interface/transceivers/MAX22025.html and https://www.ftdichip.com/Support/Documents/Da...

0693W000004KPkyQAG.png 0693W000004KPrGQAW.png
RWedu.1 by Associate II
  • 9688 Views
  • 8 replies
  • 0 kudos

STM32L476 LPRun Mode external clock source Frequency

I'd like to you a STM32L476 continuesly in LPRun Mode with external Oscillator Frequency of 2.048MHz. But in "Reference Manual" of STM32L476 is written following: "5.3.2 Low-power run mode (LP run)To further reduce the consumption when the system is ...

MGehr.3 by Associate II
  • 1158 Views
  • 1 replies
  • 0 kudos

Abnormal delta of TSC after exiting STOP mode

Hi,MCU: STM32L072MCU is using TSC and ST touch sense library. Before entering stop mode, the delta of touch key without pressing is normal (-2 to 2). However, after exiting STOP mode and then calling tsl_user_Exec_IT(), there is strange value delta.B...

John_1992 by Associate II
  • 1562 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.