STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! I'd like to use the same firmware for different types of MCU.

Hello everyone,​​I faced a shortage of MCU materials.So I found an MCU that uses the same pin map.I would like to change STM32F767IIT to STM32F767IGT.​Please let me know if the change is okay.Clock does not work when using STM32F767IGT. If...

hjuns by Associate III
  • 1864 Views
  • 3 replies
  • 0 kudos

Resolved! Range of temperature using NUCELO-F439

Hello,I am using right away a Nucle-144 smt32f439ZI for a specific development. I have red in the datasheet, the µC can be used in a temperature range of -[40, +105°]. But I didn't see anywhere the same characteristics for Nucleo-144. Any idea? Than...

LBadi.1 by Associate II
  • 1686 Views
  • 2 replies
  • 0 kudos

Transfer from STM32f411RE to STM32F411ce

Hi there,Recently if done a project regarding custom hid on a STM32F411RE Nucleo prototype board, this was successful. I have created my own pcb design but unfortunatly due the lack of availability of the STM32F411RE i was forced to go with the STM32...

MHovi.1 by Associate II
  • 5816 Views
  • 15 replies
  • 0 kudos

Peak Current Control with Slope Compensation on F334 MCU

Hi all​I'm currently implementing a peak-current control algorithm on a F334 MCU. However, I'm struggling with the implementation of the slope compensation described in the AN4885 application note (page 9-10). I would be very grateful if someone coul...

LCapp.1 by Associate
  • 905 Views
  • 0 replies
  • 0 kudos

STM32H753 Unable to transmit CAN frames

I'm trying standard CAN communication from a STM32H743 Nucleo board, with an MCP2551 CAN transceiver connected to PA11/PA12. However, I'm not able to transmit anything.With this same transceiver circuit, I am able to transmit CAN frames when connecte...

Ivo by Associate II
  • 2377 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.