STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Conflict in the definition of VTOR register

Hi.In PM0214 programming manual page 40 it says:On system reset, the vector table is fixed at address 0x00000000. Privileged software can write to the VTOR to relocate the vector table start address to a different memory location, in the range 0x0000...

Why is RCC MCO config affecting other pins?

 I'm using a nucleo F446RE. I want to set up MCO1 as 42MHz output. CUBEmx generated the the HAL_RCC_MCOConfig function below.void HAL_RCC_MCOConfig(uint32_t RCC_MCOx, uint32_t RCC_MCOSource, uint32_t RCC_MCODiv) { GPIO_InitTypeDef GPIO_InitStruct; ...

0693W00000D1vfoQAB.jpg 0693W00000D1vfPQAR.jpg 0693W00000D1vfZQAR.jpg
ZHama.1 by Associate II
  • 1495 Views
  • 0 replies
  • 0 kudos

DAC with DMA not working for STM32H753VIT6

Hi there,Here is the code for DAC with DMA. I can not see the error in the code. I have been looking at the oscilloscope for the sine wave but it is not coming. I tried without DMA, and works nice. But the DAC with DMA is not working. Please someone...

TPanc.1 by Associate II
  • 6957 Views
  • 10 replies
  • 0 kudos

How to generate SEV between cores in the STM32h745 / 747?

Hello!Currently i am working with the STM32h745 dual core MCU, i am tring to create somekind of synchonization between the m4 and the m7 cores.for that i want to utilize the SEV. i already enabled the proper iterrupts in both cores.my question is how...

yuri CH by Senior
  • 1499 Views
  • 1 replies
  • 0 kudos

SPI3 does not function for STM32H753VIT6

Hi there,Here are the two lines which I am using for SPI communication.while(HAL_SPI_GetState(&hspi3) != HAL_SPI_STATE_READY); HAL_SPI_TransmitReceive(&hspi3, (uint8_t *)& ADC_write, (uint8_t *)&ADC_read, 4, 100);The drier derived from CubeMX is not...

TPanc.1 by Associate II
  • 1930 Views
  • 3 replies
  • 0 kudos

STM32F412 CAN filter configuration

Hi,I am using STM32F412 and want to receive CAN message of both 11 bits and 29 bits ID, can i configure CAN filter to separate out the 11 bit and 29 bit IDs.Regards,Jignesh Gohil

JKG by Associate
  • 765 Views
  • 0 replies
  • 0 kudos

Resolved! Is it possible to use the RTC alarm signal on the tamper pin in order to turn on a transistor or maybe hold that value in a D flip flop?

I've been doing a lot of research concerning Low power modes for the stm32 bluepill and I was wondering if i could power my board through VDD and execute a code through it and then right after going into sleep mode I would use a switch to only power...

HAbay.1 by Associate III
  • 1172 Views
  • 1 replies
  • 0 kudos

Hello, I am using STM32L053 nucleo board. I am trying to read Multiple ADC Channels but values are not coming correct. Here is my code in details. I am using continuous mode using polling method.

#include "main.h"#include<stdio.h>ADC_HandleTypeDef hadc;UART_HandleTypeDef huart2;void SystemClock_Config(void);static void MX_GPIO_Init(void);static void MX_USART2_UART_Init(void);static void MX_ADC_Init(void);int main(void){ HAL_Init(); SystemCloc...

Resolved! Multiple ADC channels on STM32L072xx

I am using STM32L072xx module and I would like to use ADC4, ADC5 and ADC 17 (Vrefint) at the same time. But I want to use ADC4 with DMA of buffer size 500 or more. It is not necessary to store ADC5 & ADC17 in DMA.Can I use DMA only for ADC 4 and dump...

CDesh by Associate III
  • 8429 Views
  • 11 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.