STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L562E-DK VCP UART. TX OK. RX NO

Hello, guys!My name is Luis and I bought the board STM32L562E-DK for testing purposes for a new project.I have been executing many examples based on freertos and I am very happy on how the STM32L562Q could be my solution in a future project.However, ...

Llope.3 by Associate
  • 3624 Views
  • 3 replies
  • 0 kudos

MODBUS ERROR-RS485 Converter_ Reg

Hi, I am having data transfer problem with Modbus only when I use a specific RS485 Converter .I am using STM32H750VB as my main IC for a fuel dispenser project. I am having a problem with my MODBUS based on the RS485 converter.i)If i am using...

FDCAN with stm32h7451z in CLASSICAL FRAME mode

Hi there,I have problems when I m using the FDCAN controller. I m using the NUcleo STM32h745ZI with a shield with a can controller on in CLASSICAL CAN mode (NO FDCAN).If a run an example in the HAL_Driver folder it works ( @1MHz Fdcan kern freq = 40M...

DVicc.1 by Associate II
  • 1520 Views
  • 1 replies
  • 0 kudos

Start ADC from timer external input

Hello,I'm working on a nucleo-f401re board, with HAL library.I'm trying sampling a signal and measure its duration, to do it I'm triyng to use the TIM2 of my board to detect rising and falling edges of the start signal, and this works fine.I would al...

CCont.3 by Associate
  • 1273 Views
  • 1 replies
  • 0 kudos

Resolved! H743 480Mhz, VCO freq impossible?

Does anyone know how you're supposed to get a clock speed of 480Mhz when the lowest PLLP1 divider is 2, and the max "wide" VCO freq (Input source / DIVM1 * DIVN1) is 836Mhz? Ie This seems to cap the max speed at 418Mhz. Of note, Cube doesn't complain...

DOCon.1 by Senior
  • 1804 Views
  • 7 replies
  • 0 kudos

problem with nrf24l01 and stm32 wrong address value is sent

hi I used the code in this link https://github.com/MYaqoobEmbedded/STM32-Tutorials/tree/master/Tutorial%2024%20-%20NRF24L01%20Radio%20Transceiverfor communicating with nrf24l01 with stm32 and it worked fine but I wanted to rewrite it in register leve...

salar1991 by Associate II
  • 1928 Views
  • 2 replies
  • 0 kudos

UART at slow rates: How stupid just I am

I've just been caught by this very same issue:https://community.st.com/s/question/0D50X00009XkaBXSAZ/rm0090-usart-minimum-attainable-baudrateAt this place I'd like to ask ST to reconsider baudrates generation for both UART and SPI - please connect th...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.