STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

The DMA buffer configured with a multichannel ADC setup ( Processor STM32f769II) shows values in different buffer location with respect to the rank configured in the ADC setup. How can this be fixed?

We have connected 7 channels in ADC2 to a STM32F769II processor. The DMA to ADC is enabled and the rank for conversion too is configured. But on testing, the ADC values are being shown in buffer location very different from its rank.This happened in ...

SP.7 by Associate
  • 782 Views
  • 0 replies
  • 0 kudos

STM32L496RET6

please let us know the availability of STM32L496RET6 controller

APara by Associate II
  • 1274 Views
  • 2 replies
  • 0 kudos

MCU : stm32h743ii. two usart problem

i use two uart.(usart1 & usart2).when i receive data(usart1), first, the program will into "void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)".but when i i receive data(usart2), second, the program will not into"void HAL_UART_RxCpltCallback(UA...

RLiu.11 by Associate II
  • 1278 Views
  • 3 replies
  • 0 kudos

SPI DMA fails (only) with ICache enabled, why?

I have a project which uses SPI DMA, and the SPI DMA appears to fail when I enable the instruction cache (ICache! not DCache), but otherwise appears to work perfectly fine. I do observe this for both a F722ZE and G491RE.I'm working on this since 3 we...

waldmanns by Associate II
  • 3684 Views
  • 6 replies
  • 0 kudos

STM32L4R5 not always booting after nRST

We are seeing an issue with the STM32L4R5ZI that does not boot 100% of the time if nRST is asserted after powering up (i.e., pressing and releasing reset button). We have seen this issue with the Nucleo board and with two different boards we made our...

RDowl.1 by Associate
  • 1293 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H743ZI Direct channels for ADC.

Hi,I am using STM32H743ZI micro controller of LQFP144 package. My doubt is that in the data sheet they are mentioning that it has 2 direct channels for ADC but they are not mentioning what are the channels or pins offering thisThey are only talking a...

GHARI.1 by Associate II
  • 1355 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.