STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to program an STM32H73x to put it in low power, that it consumes as little as possible, and that it can wake up with a GPIO?

I am using an STM32H735G-DK board to do my tests. My goal is to toggle a LED on PC2 every time I wake up the MPU when I put PG5 to ground. Once the LED is toggled, I want the MPU to go to the lowest possible power consumption. Does anyone have an exa...

BenBel by Associate II
  • 1474 Views
  • 2 replies
  • 0 kudos

Order of ADC calibration step

The errata sheet of the STM32L476VG states: I wonder if the order of the ADC calibration step is important. I was performing the following steps:1- Set ADC clock source2- Enable ADC clock3- Disable deep power mode (ADC1 and ADC3)4- Enable ADC voltage...

0693W00000GW1ttQAD.png
xpp07 by Senior
  • 1949 Views
  • 1 replies
  • 0 kudos

HI, I use cubeIDE. I was trying to use NVIC functions such as NVIC_SetPriority(EXTI1_IRQn,1), but the function and EXTI1_IRQn are not recognized, and it gives me an error. is there is a header file that I should add? Thanks very much.

I am trying to write the drivers for stm32f401 nucleus without using HAL and by writing to registers directly. when I created the project I choose the target project to be empty instead of STM32Cube To make sure I do not add HAL drivers. I know there...

0693W00000GW0QCQA1.png 0693W00000GW0Q7QAL.png
SElkh.1 by Associate
  • 1480 Views
  • 2 replies
  • 0 kudos

Voltage with DACs unstable

I'm using the DACs of STM32F303K8. The max voltage of the DAC1 is 3.3V but the second is 3V.I don't find any explanation for it and it looks like also quite strange.​PS. To my nucleo is not. Connected to any Vref. It is necessary?​Anyone can help me?

FTrom by Associate II
  • 5917 Views
  • 18 replies
  • 0 kudos

STM32H723ZGT6 accidental Vcore overvoltage

Hello,I designed a custom board with an STM32H723ZGT6.It worked fine, then, long story short, this happened:I accidentally connected the VCAP pins (Vcore voltage) to 3.3V, then switched the board on. After about 2...3 seconds I realised something is ...

vjaz by Associate
  • 1533 Views
  • 2 replies
  • 0 kudos

Need for Speed Using STM32 SPI with DMA to W5500.

I am porting the code from ATMega128 to STM32F103 for faster throughput to WIZNET W5500 using the WebServer.C for ATMega128. I am using the HAL coding as I am new to STM32. While the throughput is faster than the ATMega128 but I need more speed. Cha...

CK.3 by Associate III
  • 8367 Views
  • 9 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.