STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F103 runs only after flashing and not after that

I am using STM32f103 and Cubemx ide. I implemented small project 1 month back and that time it was working fine but now when i am trying to use same code then i observed weired behaviour.Code runs only after binary flashing and after that if i press ...

SS.Sagar by Associate III
  • 2330 Views
  • 3 replies
  • 0 kudos

Resolved! STM32 gpio maximum toggling speed

Hi,I my project I need to toggle a gpio pin at 200MHz or more than this.Which STM32 controller is peferable.please any one help me.thanks and regards

Trinu by Associate III
  • 1812 Views
  • 1 replies
  • 0 kudos

Resolved! ADC external trigger features in STM32F103C8T6

Currently working with a STM32F103 MCU for a power metering application.In order to have a programmable time shift between sampling voltage & current , i decided to use a PWM signal from the Timer to clock the ADCs.I wanted to kick the ADC1 at the ri...

MBenh.1 by Associate
  • 2196 Views
  • 2 replies
  • 0 kudos

Help please, how to debug in SDRAM with IAR?

I am developing with stm32h750.My application is storaged in QSPI Flash and running in SDRAM.I use a bootloader to move image from QSPI Flash to SDRAM and​ jump to image.For downloading, i made a cmd line tool to communicate with bootloader via seria...

LHuaf.1 by Associate
  • 1130 Views
  • 0 replies
  • 0 kudos

Known issues with D-cache and FMC on STM32F7

Hi,I'm using a STM32F765 clocked at 216MHz and when D-Cache is enabled it badly affects reads from a device connected via the external FMC address/data bus (NE1, 16 bit data, 10 bit address). The following pictures show the problem (note ringing is c...

0690X00000Buz5hQAB.jpg 0690X00000Buz6zQAB.jpg 0690X00000Buz7EQAR.jpg
dave2012 by Associate III
  • 6724 Views
  • 12 replies
  • 0 kudos

Resolved! Problems editing a question here at stm community

When i try to edit the content of this two months old question of mine i get this error without changing its contentError while parsing Rich Text Content: Unsupported HTML tag or attribute encountered - data-fileid

0693W00000GYhceQAD.png
Javier1 by Principal
  • 1269 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.