STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7 dual core - M4 SPI Issue

After configuring SPI channel on the M4 core as a read only master (while observing signals on the scope) I was not able to generate a clock while using the  HAL_SPI_Receive() functions (which returned HAL_ERROR status). When I changed the configurat...

yuri CH by Senior
  • 1092 Views
  • 1 replies
  • 0 kudos

how to use just Rx pin of an uart

Hi, I have a sensor that send data over uart to a stm32f722 uC. This sensor is powered at the same time of uC. I've noticed that some times the sensor stop sending data. For example, if the code is running ok and then reboot the uC some times the sen...

Lgarb.1 by Associate II
  • 3338 Views
  • 2 replies
  • 0 kudos

STM32F767ZI UART DMA RX LOCK(STOP)

After system initialization, UART DMA Rx function is normal.When time passes, data is not received in the DMA buffer and the phenomenon is stopped.To solve the problem, we checked the normal operation by repeating the DMA initialization as shown belo...

Snam.2 by Associate
  • 2533 Views
  • 4 replies
  • 0 kudos

Resolved! Why is there corrupt data when sending as SPI Slave?

Hello!I have been trying to configure the STM32F407VE as a SPI slave. My first time configuring a SPI device ever so its all new to me. You can see my SPI settings and code as an attachment.I am using software SS as I only have one slave and one mast...

JCorl.1 by Senior
  • 12018 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.