STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Using "HAL_CAN_AddTxMessage" from interrupt and main loop

Hi, I want to be able to add CAN message with "HAL_CAN_AddTxMessage" from interrupt and main loop (loop maybe busy sometimes so I cant send all messages from it). I assume they can collide and override so its not safe to do it from both?What are my o...

JBond.1 by Senior II
  • 925 Views
  • 0 replies
  • 0 kudos

Resolved! polling interrupt flag, without activate interrupt

I was working with SPI dma transmision. I config two channels for transmit and receive, however I didn't enable interrupt option in dma, however, before each transmision I cleared tc flag, and then enable spi while polling the tc flag. This works rea...

JCuna.1 by Senior
  • 1107 Views
  • 1 replies
  • 0 kudos

H743ZI Full-duplex DMA communication. When the baud rate is 25M, the master and the slave can receive the data correctly. When 50M and 100M, the slave can receive the data correctly, but the master cannot receive the data correctly.

Use two NUCLEO-H743ZI boards for SPI communication. Full-duplex DMA mode. When the baud rate is 25M, the master and the slave can receive the data correctly. At 50M and 100M, the slave can receive the data correctly, but the master cannot receive the...

one V by Associate III
  • 1235 Views
  • 1 replies
  • 0 kudos

STM32F407 DISC-1 out of stock

Hello, In India, the STM32F407 discovery board is out of stock. I enquired many vendors like element14, Digikey and other locals, it's not at all available. Did ST stop the production of this ? Will it be availabel in the future ? which is the close ...

n.serina by Associate III
  • 2833 Views
  • 4 replies
  • 0 kudos

Resolved! Hardware trigger for MDMA?

Hello there.Our design currently utilizes MDMA for intensive writes from SRAM4 to FMC bus area. Transfer is setup with double word transactions, witch is critical for performance. DMA 1/2 or BDMA is simply do not cut it due to lack of AXI access i gu...

BStud.1 by Associate II
  • 2866 Views
  • 3 replies
  • 0 kudos

Does the STM32F413 use the LSE generation 1 or 2?

The document AN2867 (Oscillator design guide for STM8AF/AL/S, STM32 MCUs and MPUs) defines to groups for the F4 series: F4_g1 and F4_g2. There is a list with the controllers for each group, but the STM32F413 is not mentioned.

Stefan W by Associate II
  • 2012 Views
  • 4 replies
  • 0 kudos

Problem with STM32H743ZI2 USART Rx DMA

Hi,Can someone help me identify what I am doing wrong ?Still having issues with the DMA, but with Rx DMA instead. The issue with Tx DMA is fixed.I am trying to send 4 chars from a terminal to the H743 rxbuf array using DMA.In the debugger window, the...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.