STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32G0B1 programming Option Bytes stopped after OBL_Launch

The MCU stops when the program reaches this line (FLASH->CR |= FLASH_CR_OBL_LAUNCH;) in the function below.The option bytes I want to write are at the moment still unchanged to the delivery state. Later they will be changed to RDP Level 1.void Option...

FRieb.1 by Associate III
  • 4530 Views
  • 5 replies
  • 0 kudos

UART RX Interrupt disable

Hello,I want to disable the uart rx interrupt during transmitting the data like the following flow.UART Rx interrupt disable(Only uart rx interrupt)UART Data TxUART Rx interrupt enableWhich HAL Library I could use for this process?Thanks

Kim.Andy by Associate III
  • 4280 Views
  • 1 replies
  • 0 kudos

stm32f373r8t6 - CAN not working at 1Mbit / s

Hello forum users!Created a project by example[url] https://istarik.ru/blog/stm32/159.html [/ url]Slightly corrected, so that a new frame is sent every 10 msec.The project works at (except one) any speed (100kbit - works, 500, 800 - works).Data is tr...

how to transmit data via SWO STM32H743

I can not start transfer via SWO to STM32H743.Port PB3 initialized clock feed.Initialized SWO:*(__IO uint32_t*)(0x5C001004) |= 0x00700000; // DBGMCU_CR D3DBGCKEN D1DBGCKEN TRACECLKEN //UNLOCK FUNNEL *(__IO uint32_t*)(0x5C004FB0) = 0xC5ACC...

LJack.3 by Associate
  • 1983 Views
  • 2 replies
  • 0 kudos

NUCLEO-F303K8 external power supply not working

Hello to everybody,I have the NUCLEO-F303K8 and I'm trying to use an external power supply (+5V).As it is described in the reference manual MB1180, section 6.4.2, the external 5V needs to be connected to the +5V connector (pin 4 of CN4).However, by d...

frnt by Senior
  • 1793 Views
  • 3 replies
  • 0 kudos

STM32H743 SPI DMA NOT WORKING, CACHE DISABLED

Hi everyone,I have to port one proyect from a STM32F4 to a STM32H743. In this project it is important to use the SPI through DMA, so after reading a bit about the DMA-Cache issue in this microcontroller i decided to disable the D-Cache in order to ma...

0693W00000GZtZeQAL.png
DCajigal by Associate III
  • 2584 Views
  • 3 replies
  • 0 kudos

Parallel NOR flash for extra code memory

Hello,I'm using STM32H753-Eval2 board wherein MT28EW128ABA1LPC-0SIT NOR flash is connected over parallel interface(FMC mode). I want to keep some part of application code into this parallel flash, I've referred one application note from Keil which wo...

0693W00000Ho04QQAR.png 0693W00000Ho04GQAR.png 0693W00000Ho04BQAR.png
AShel.1 by Associate III
  • 1265 Views
  • 0 replies
  • 0 kudos

Resolved! LPTIM with external clock (no synchronization – STM32L0)

Dear all,I am working on a project with an L081KZ and want to count pulses with a frequency higher than the clock. In the post here (community.st.com/s/question/0D53W00001EyzG5SAJ/) I thankfully got the tip to use the LPTIM as it has an asynchronous ...

0693W00000HntvSQAR.jpg
ToStei by Associate II
  • 3433 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.