STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! QSPI of STM32L496A

Hi I have interfaced STM32L4 qspi with Winbond(W25N01GV). I am using HAL api's. The problem is erase/write to a page(2KB) address(say 0x0) repeats to the page after 512 KB(Say 0x80000) and so on. This is a 128 MiB NAND flash and erase command(D8h) o...

Vsv.1 by Associate II
  • 11306 Views
  • 24 replies
  • 0 kudos

32F417 SPI running at half the speed it should

Hello,I am using a chopped-down function from the Cube HAL code to talk to a serial FLASH. The original function has a mass of options which were checked at runtime - the usual thing for HAL code...It's all working fine. SPI2, 21MHz (the fastest I ca...

PHolt.1 by Senior III
  • 8403 Views
  • 25 replies
  • 0 kudos

How to develop a product?

How to develop an Embedded System around STM32 MCU from scratch efficiently on the first attempt? For Eg. Developing a system with ADC, CAN, RS232, SPI, I2C, UART around an ST Controller efficiently? Developing a system according to the product requi...

sanket47 by Associate II
  • 5292 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.