STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

May someone help explain what are TIM1_CH1 or TIM1_CC1 ?

I am using the STM32F407Zg MCU and is learning how to set up the ADC for continuous sampling by timer. But I have trouble to understand the manual. The ADC section refer to TIM1_CH1 or TIM1_CC1 etc. But the Timer section do not use the same term.

nNg.1 by Associate II
  • 4021 Views
  • 6 replies
  • 0 kudos

Keil: SWDIO no target connected

Posted on February 19, 2018 at 14:48I'm using a stm32f407vg board. Suddenly I can't download my code to flash memory anymore. I'm using the keil toolchain. I tried stm32 st-link utility, but it can't connect to target either. I tried the option 'con...

Resolved! I2C SCL no clock

Hello, I am trying to get my I2C code Master working. I don't have the slave device connected and I am trying to see the output on a logic analyzer. I have connected the SCL and SDA pins to breadboard to a 2k pull up of 3.3V and the board is running ...

0693W00000JNRAoQAP.png
VThan.2 by Associate III
  • 4303 Views
  • 7 replies
  • 0 kudos

STM32 U575 ADC1 differential channel configuration

I am having some difficulty configuring STM32U575 ADC1 for Differential inputs. The reference manual and auto-generated code seem to have conflicting information:The ADC1 Connectivity diagram from Reference Manual (below) indicates configuring Channe...

0693W00000JNRSdQAP.png 0693W00000JNRRzQAP.png
Tvoge.1 by Associate II
  • 2461 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.