STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How can I calculate and set blanking window width of COMP1?

I have an SM32H723 NUCLEO-144 board. I successfully implemented COMP1. It works, but I have some bouncing at the rising and falling edges (100Hz signal). I found a COMP_OutputBlanking example for NUCLEO-H7A3ZI-Q (No blanking example for NUCLEO-H723ZG...

Louie88 by Senior II
  • 1903 Views
  • 1 replies
  • 0 kudos

F411 LL SPI-DMA callback delay too long

My code is based on LL SPI-DMA example.The original code does not have chip select, so I use one GPIO pin as CS pin. /* Start SPI Tx/Rx */ ADC_CS_Low();   /* Enable DMA Channels to start Tx/Rx */ LL_DMA_EnableStream(DMA2, LL_DMA_STREAM_2); L...

HDaji.1 by Senior
  • 1930 Views
  • 4 replies
  • 0 kudos

STM32 PWM to analogue output converter circuit?

STM32 TIMER PWM (10KHz) very duty cycle for very output voltage.now i want (0 - 10V DC) analogue output voltage is very by changing duty cycle of TIMER PWM (0 - 100 % duty).what is the circuit diagram for PWM IP to ANALOGUE OP?so for example: 10V DC ...

SystemClock_Config() runs over and over

Im using a STM32L412, I've made the config in STMcube but when I run the program (no main code, just the setup routine) it never reaches the main loop. By placing breakpoints I have deduced that  SystemClock_Config(); runs over and over again. It see...

deep_rune by Associate III
  • 2384 Views
  • 3 replies
  • 0 kudos

Flash erase is unreliable on STM32H743 (Code Provided)

Hello All,I am working with an STM32H743 and am having issues reliably erasing flash (unreliable in that it fails ~95% of the time). The code which erases flash runs from RAM (functions are allocated in RAM). I disable many of the interrupts before e...

0693W00000KaJoHQAV.png
AAgar.2 by Associate III
  • 8151 Views
  • 11 replies
  • 0 kudos

Why does the execution time of STM32F767ZIT6 (used in NUCLEO-F767ZI) not grow as expected when the amount of code to execute increases?

I measure the execution time of a function by putting the toggle of a digital output and the function call into a cycle and measuring the period of the square wave at the digital output with an oscilloscope. The execution time is half a period. To te...

Silvano by Associate II
  • 13251 Views
  • 26 replies
  • 0 kudos

Sram 10 megabytes

Hello... Tell me, is it possible that microcontrollers with sram 10 megabytes and more will appear soon?

MTS by Associate II
  • 2297 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.