STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 HAL library build errors.

I am getting compile error in a lot of HAL files (gpio, rcc , spi). The error is for registers and peripherals which are not present in F407 but are present in F42/43 like. Since the HAL files are common for whole F4 series, these regs and functions ...

NKunwar by Associate II
  • 6913 Views
  • 7 replies
  • 0 kudos

F411 SPI LL example: problem when changing SPI1 to SPI4.

I tried to change SPI1 to SPI4 in the LL example code.My problem is I cannot detect any signal on the CLK or data pins.void Configure_SPI4_DMA(void) { /* DMA2 used for SPI4 Transmission * DMA2 used for SPI4 Reception */ /* (1) Enable the cl...

HDaji.1 by Senior
  • 3406 Views
  • 12 replies
  • 0 kudos

The iOS "ST BLE Sensor" App is crashing when you press connect in that App. Version 4.14.5 available in US Apple App store. 100% repeatable bug.

Android version fails to connect with "error during the connection with the node XYZ". I have tried both latest version available in Google Play Store (v4.14.7) and the other version (v4.14.4) available on ST Micro website. Does anyone have solutions...

Arthur1 by Associate
  • 747 Views
  • 0 replies
  • 0 kudos

Resolved! Wake up immediately after shutdown in STM32L451

HAL_PWR_EnterSTANDBYMode() will still wait properly, but HAL_PWREx_EnterSHUTDOWNMode() will immediately return to RUN mode.What do you think is the cause of immediate wakeup?​As shown below, the only code difference is whether to enable HAL_PWREx_Ent...

Yoshi1 by Associate III
  • 1726 Views
  • 2 replies
  • 0 kudos

Resolved! STM32L476JG DMA MEMORY ---> SAI2-A

Have a file and I am trying to transfer it to SAI2. For some reason ???? I am not getting into the DMA Callback. DMA is in normal mode. Can anyone shed any light on this? /* USER CODE BEGIN 2 */ HAL_DMA_RegisterCallback(&hdma_sai2_a, HAL_DMA_...

SWenn.1 by Senior III
  • 1549 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.