STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HAL-Lib MPU Configuration Question

Hello,I would like to know if there is a possibility to readback the MPU confiugration for each configured region? HAL only provides a setter function. If I take a look into the internal implementation, it seems that regions get overwritten, when I ...

Floki.1 by Associate II
  • 872 Views
  • 0 replies
  • 0 kudos

STM32H745I-Disco PWM Input Frequency Not detecting

Hi, I am trying to detect a 3v PWM frequency with my STM32, I have my live expresions setup for my variables, but the values do not budge from 0. Im sure it is something up with my code. Any help would be appreciated cheers.

CChri.5 by Associate III
  • 3168 Views
  • 6 replies
  • 0 kudos

3-Wire SPI to demo board not working?

Good afternoon.I have configured SPI2 on STM32L476RG as Master Half Duplex, clock = 4MHz, CPOL = 1, CPHA = Edge 2. I am connected to a Pololu 2736 demo board (LSM6DS33). The timing diagram for the part shows resting clock as high (CPOL = 1) and MIS...

0693W00000KcO0QQAV.png
SWenn.1 by Senior III
  • 1039 Views
  • 1 replies
  • 0 kudos

Does anyone know when STM32 MCUs are going to be available on the market? Is there any estimate time known?

Well, I know that this is the most commonly asked question these days, but let me please ask it. Maybe it will help me and future readers of this post.I was working with STM32 MCUs for a quite long time, works great and it is planned to use new versi...

using stm32h747. I am reading ADC data using SPI on ADS8661 IC. the sampling rate we are able to read at is 14us using FOR loop(PFA). trying to reduce the sampling rate by DMA receive through tim12 trigger, not working, please guide me how to in cube mx

for(int i=0;i<3000;i++) { //__HAL_TIM_SET_COUNTER(&htim4,0); while(!(GPIOI->IDR &(1<<5))); //monitoring RVS Pin GPIOI->ODR &= ~(1<<0); // CS pin Low HAL_SPI_Receive(&hspi2, data_rcv ,2,1); // reading 2 bytes at a time GPIOI->ODR |= 1<<0; //CS ...

VV.29 by Associate
  • 1312 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.