STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F103VBTx GPIOC pin3 Pulling up first and then down will result in failure to receive CDC data within 100ms,Probabilistic

Hi​:STM32F103VBTx STM32CubeMX_v5-3-0The basic code is generated by cube.​There are the following changes:​static int8_t CDC_Receive_FS(uint8_t* Buf, uint32_t *Len){  /* USER CODE BEGIN 6 */ CDC_rx_len += *Len;//pinjie    USBD_CDC_SetRxBuffer(&hUsb...

xhan.11 by Associate II
  • 2004 Views
  • 4 replies
  • 0 kudos

Resolved! What is the value of R_ADC in STM32G474 (the resistance of ADC multiplexors)? The datasheet does not list this parameter.

The application note AN2834 states that this parameter should be listed in the device datasheet. This is true for MCU families like F4, but not for G4. I know that there is a difference between slow and fast channels, but where could I find precise v...

VMich.1 by Associate II
  • 4679 Views
  • 5 replies
  • 0 kudos

USART DMA Problem

I' using USART1 to send and receive DMA with a module. When I configure DMA for one of TX or RX, it works fine. but when I configure it for both TX and RX, in RX-Buffer I have '\0' character in second position. for example the receive buffer is so:"...

Slh by Senior
  • 1466 Views
  • 2 replies
  • 0 kudos

I want to use CCMRAM in 407. Is there a possibility of getting malloc to allocate CCMRAM instead of regular RAM? I changed the linker script to put stack and heap in CCMRAM but the issue is CCMRAM clock has to be enabled before any call takes place.

To overcome this problem I modified the start up assembly file by enabling the clock (AHB1ENR bit 20) at the very beginning. The program which was freezing before enabling the clock started working but stops/freezes after executing a few C statements...

how to write in external flash memory with stm32l4?

HII am using stm32l496 and want to use external flash memory MX25R6435F .Although this memory has 64 MB of memory, I set it to 8 MB in the ioc file and mx25r6435f library, but when I write in that string or character, it is not written correctly and ...

alianvari by Associate III
  • 3867 Views
  • 2 replies
  • 1 kudos

Since the PIN of STSPIN32F0 is not enough, it is implemented to view log messages using PA14 (SWD_CLK) as UART.

Since the PIN of STSPIN32F0 is not enough, it is implemented to view log messages using PA14 (SWD_CLK) as UART.But after that, I can't download it, so please inquire.​1. Could you explain that re-download the MCU in this state?​2. I don't have any PI...

dkwon.2 by Associate
  • 1102 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.