STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

how to flash/ update STM32 firmware

Hi there,I would like to ask for some help or advice to fix the below:I want to flash/ update the firmware (.dfu file) of my LILYGO TTGO T-Motion/softRF Dongle which runs on STM32 S76G Lora Chip by using DfuSe DemoUnfortunately the device is recogniz...

ADros.1 by Associate II
  • 13348 Views
  • 6 replies
  • 0 kudos

Resolved! STM32H7 Delay Block Configuration (LNGF does not get set)

Hi, I was trying to configure the Delay Block on the STM32H723xx for the Octo-SPI (in my case OCTOSPI2). The datasheet documentation on that part is quite simple with 6 steps, but I get stuck at the Line Length Valid Flag. After the first round (unit...

JRS by Associate III
  • 7690 Views
  • 10 replies
  • 1 kudos

DMA interrupts don't work

Microcontroller STM32F401. The DMA controller transfers data from memory to the DR register of the SPI interface. With the HTIE and TCIE bits set, DMA is not included in the interrupt handler. At the end of the data array transfer, the program freeze...

Vlad2022 by Associate II
  • 9050 Views
  • 18 replies
  • 0 kudos

Resolved! Why does a condition always evaluate to be true?

Hello everyone,I have an issue regarding an always true condition produced by the following code.Since I have never run into this kind of issue with C I guess it must have something to do with the STM environment.The condition within the if-statement...

JHarm.1 by Associate
  • 2194 Views
  • 2 replies
  • 0 kudos

Receive command UART polling mode using LL library

Hi everyone!I've been trying to implement UART reception using LL library in polling mode. The code below is what handles the reception: uint8_t LL_USART_Receive_Byte(USART_TypeDef *USARTx) { // Wait for Read Data Register is not empty while (!LL_U...

MCUnoob by Associate II
  • 6382 Views
  • 7 replies
  • 2 kudos

Need more understanding about the Timer enabling fn I am changing CNT register of the Timer in order to get a changed time period on the go (for down counting mode), but doing so correctly is getting delayed by one period.

So I am using STM32H725 on which I have Timer 2 (general purpose timer) which is in down counting, one pulse mode with an interrupt which is triggered at underflow. Once the interrupt is fired, the TIMx_CNT register value is changed and then __HAL_TI...

0693W00000LyvUMQAZ.png
Akshat1 by Associate II
  • 2911 Views
  • 5 replies
  • 0 kudos

Resolved! which STM32L412 MCUs have SMPS and are in production

Hello,according to the product selector on the ST website, the only MCU from L412 series that has SMPS and is in production is STM32L412RB with 64 pins in LQFP and UFBGA package.In the product specification v6, on p57 at the PIN definitions table, I ...

wyv by Associate II
  • 5763 Views
  • 11 replies
  • 0 kudos

Avoiding STM32 for new product designs?

Is it reasonable to consider using an STM32 for new product designs. Can't find any official statements of if and when any microcontroller will be available through official channels/distributors.

BenRegal by Associate
  • 2072 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.