STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

the max frequency of STM32G030x6x8 series CORE

hi,everyone,I'm a new user of the SMT32 MCU, now i'm looking up the datasheet of STM32G030x6/x8 series, In this article, the Frequency of CORE is described to reach up 64MHz on PAGE 1, but on PAGE 11, Figure 11 block diagram, fmax = 56MHz, so what ...

Start condition for I2C not working.

I am using an STM32F411, and am attempting to use I2C to communicate with an MPU-6050 (relevant datasheet info attached).I've tried to setup I2C in accordance with the timing requirements on the MPU-6050 datasheet: #define MPU6050_PIN_CL (6) #de...

0693W00000NqomBQAR.png 0693W00000NqomGQAR.png
Starman by Associate II
  • 3763 Views
  • 5 replies
  • 0 kudos

How to port the NFC Reader Library to the STM32 environment?

Hi Community :)I currently using the NXP CLEV6630B RFID reader (chip is SLRC610) for our medical project, and I am using STM32H7 as a host microcontroller.Did anyone do something like that and has ported the NXP reader library to match the desired en...

Liad by Associate
  • 1404 Views
  • 0 replies
  • 0 kudos

I2C - Adding a registry & value.

Hi, I want to try sending data to a slave consisting of several registries and have seen code example:-uint8_t buf[2];buf[0] = register_addr;buf[1] = data;HAL_I2C_Mem_Write(ftHandle, slaveAddr, buf, 2, timeout);Would this work in practice? As it is m...

PLee.3 by Associate III
  • 1699 Views
  • 3 replies
  • 0 kudos

Bitfield registers acess

Hello I am not very familiar with the Low-level stm32F register,I have a question about the definition of each register in the  TIM_TypeDefI want to have a separate access to each bit, It is possible?I the stm32F429xx.h I have this:typedef struct{ __...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.