STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Firmware Behaviour change after files clean up

I am working on a state machine to control a stm32f334 mcu, first state would be general initialization, the wifi initialization, waiting for stable input and some other states that are not relevant here. It was working smoothly and I wanted to commi...

ISust.1 by Associate
  • 875 Views
  • 0 replies
  • 0 kudos

STM32G491 (Flash category 4): Flash IAP programming?

Hi, I would like to re-program only some higher part of flash memory with In-Application-Programming (Chip: STM32G491 - this in RefMan is defined as "Flash category 4" device).My normal firmware e. g. is running in lower 256kB Flash.And now I want to...

flyer31 by Senior
  • 1095 Views
  • 1 replies
  • 0 kudos

STM32F439ZI first embedded flash program issue

Hi,I'm working with STM32F439ZI MCU. I setted system clock 180 MHz and as Reference Manual (RM0090) says I did:-- VOS[1:0] = 0x11-- over drive mode enabling-- 5 WS latency (6 CPU cycles)When I try to program something the first time after power up, i...

AFara.2 by Associate II
  • 1913 Views
  • 3 replies
  • 0 kudos

Resolved! MCU type - Can one identify it?

Using something like STLink util or newer, command line software: Can one identify which type of STM32 MCU is connected? E.g. for use in further scripts. It doesn't help if I see it on a GUI somewhere.

Can it be possible to trigger DMA using a GPIO pin in STM32?

For my application I'm using a comparator and i have set a reference voltage(threshold) for that and my application is that, if the current passes through the threshold then my comparator output should be turn on(1 or 0). I have set the comparator ou...

SKUND.11 by Associate III
  • 3962 Views
  • 4 replies
  • 0 kudos

How to handle UART errors?

Hello!I'm receiving data in UART Rx with DMA and I need to make it inmunne to disconnections. Now, sometimes I can recover the communication after a disconnection, but I need it always.Using the debugger I realized that huart1.ErrorCode change its va...

SGonz.2 by Associate II
  • 3811 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.