STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI stops working when enable I2C?

Hello, I'm trying to use I2C and SPI simultaneously on an STM32F103C6TX.Both are working properly when only one of them is activated. However, when activating I2C peripheral with SPI already activated, SPI clock still works but the MOSI pin stops wor...

MCris.4 by Associate II
  • 3725 Views
  • 5 replies
  • 0 kudos

STM32 memory out and how avoid that

Hi there,here i'm for ask another help. I compile my program with keil and i read this data :Program Size: Code=15988 RO-data=360 RW-data=24 ZI-data=2088  How i can interpret ? I use one STM32G031F4P6 wher i have 8K of RAM and 16K of program. So i ju...

SGian.1 by Senior
  • 6710 Views
  • 11 replies
  • 0 kudos

Which STM32 controller has secure booting capability?

Im currently building boot loader to securely boot the firmware by signing the firmware images and verification during the boot of the firmware.So i'm using controllers like stm32f411,stm32f446,stm32f746 and stm32h723 ,I believe from the available do...

Yashwanth by Associate II
  • 2946 Views
  • 2 replies
  • 0 kudos

Timmer input STM32F429

Fig 9 of the STM32F429 datasheet it effectively states that the external source clock/signal has to be 1/3 of the Timer clock – makes sense as you want to ensure you capture the edge of the input signal. However, the Ref manual section 17.4.3, the re...

Reading Encoder pulses using external interrupts

I'm using STM32L451VCI6 MCU to read pulses from a rotary encoder attached to the shaft of a stepper motor using external interrupts. I'm incrementing a counter at rising edge of interrupt.According to spec of the encoder, I should be able to read 400...

NSure.1 by Associate II
  • 2884 Views
  • 3 replies
  • 0 kudos

Resolved! TCXO HSE to NUCLEO f446re

I need a accurate time source for time synchronisation between boards and timestamping of sensor data so want to add a accurate HSE. I'm currently considering a 7N-26.000MBP-T 26MHz TCXO connected to OSC_IN. I would have a 10nf bypass capacitor and d...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.