STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

error 0xfffffffe

I am writing a Programm on stm32cubeide. But during Debugging and Running the Programm, I habe the error Break at address "0xfffffffe" with no debug information available, or outside of program code.I don't know what it means and can I handle with th...

TGill.2 by Associate
  • 3069 Views
  • 2 replies
  • 0 kudos

stm32h750vbt6 DMA is not working if active D cache

I have read previous posts ,,,I set up dma to read adc ,Although dma's destination address is allocated from AXI RAM, dma does not work when d cache is active.Can anyone share detailed information or a sample code about this?

Enabling automatic, regular wakeup with RTC timer

Dear community,I have some issues with implementing an automatic wakeup with the RTC timer on my STM32L476RG (currently on the Nucleo-Board, will be later replaced with proprietary hardware). I generally have two wakeup sources: either the L476 is wo...

AHass.1 by Associate II
  • 1427 Views
  • 1 replies
  • 0 kudos

STM32f469 SDRAM Read/Write issue on FMC Bank2

Hello all,I have W9816G6JH( Winbond) SDRAM interfaced with STM32f469 on a custom board.SDRAM is interfaced on FMC Bank2.I have generated SDRAM initialization code for MDK-ARM using CubeMx. When I Write and Read back on SDRAM address 0xD0000000 it sho...

JShin.4 by Associate
  • 1307 Views
  • 0 replies
  • 0 kudos

STM32F407 - Question of how to use 3-wire SPI

Hi,My slave device has only one bidirectional data line. Now I want to configure the SPI in the half-duplex mode. And I noticed that the reference manual gave an descripiton of 1 clock and 1 bidirectional data wire.I want to ask if ST has peripheral ...

0693W00000QMnKhQAL.png
JGu.2 by Associate
  • 2538 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.